- Sat Jan 12, 2013 9:29 am
#154133
Hi,
I am trying to communicate two LPC1769 mcu by canbus. My circuit is below. For communication, i use MCB1700 board keil canbus example. I have edited the can_setup() function as below( for p0.4 and p0.5).
Until now i can not make communication. Please help me!
I am trying to communicate two LPC1769 mcu by canbus. My circuit is below. For communication, i use MCB1700 board keil canbus example. I have edited the can_setup() function as below( for p0.4 and p0.5).
Code: Select all
void CAN_setup (uint32_t ctrl) {
LPC_CAN_TypeDef *pCAN = (ctrl == 1) ? LPC_CAN1 : LPC_CAN2;
if (ctrl == 1) {
LPC_SC->PCONP |= (1 << 13); /* Enable power to CAN1 block */
LPC_PINCON->PINSEL0 |= (1 << 0); /* Pin P0.0 used as RD1 (CAN1) */
LPC_PINCON->PINSEL0 |= (1 << 2); /* Pin P0.1 used as TD1 (CAN1) */
NVIC_EnableIRQ(CAN_IRQn); /* Enable CAN interrupt */
} else {
LPC_SC->PCONP |= (1 << 14); /* Enable power to CAN2 block */
LPC_PINCON->PINSEL0 |= (1 << 9); /* Pin P0.4 used as RD2 (CAN2) */
LPC_PINCON->PINSEL0 |= (1 << 11); /* Pin P0.5 used as TD2 (CAN2) */
NVIC_EnableIRQ(CAN_IRQn); /* Enable CAN interrupt */
}
LPC_CANAF->AFMR = 2; /* By default filter is not used */
pCAN->MOD = 1; /* Enter reset mode */
pCAN->IER = 0; /* Disable all interrupts */
pCAN->GSR = 0; /* Clear status register */
CAN_cfgBaudrate(ctrl, 500000); /* Set bit timing */
pCAN->IER = 0x0003; /* Enable Tx and Rx interrupt */
}
Until now i can not make communication. Please help me!