- Tue Jul 10, 2012 5:19 am
#147227
Hello,
Since every problem so far with my setup has been solved by reading old threads from this forum I thought my hopefully last but sadly most confusing problem could be solved here as well. My problem is that after I have connected with the MCU and try to debug I get this very informative error: 'No register.'
Edit: This always happens at 27% if that might be relevant.
I'm using the following setup:
Windows XP
Eclipse IDE helios (Build id: 20100917-0705)
OpenOCD 0.4.0
GNUARM
Cygwin
Olimex arm-usb-ocd
STR H711
When connecting I get this response:
C:GNUARM\bin>arm-elf-nm.exe -n C:\projects\str_711\main.elf > C:\projects\str_711\main.sym
Here is the make file if anyone bothers to read it:
If there is any information that might be useful pleas let me know.
Pleas disregard the grammar errors, English isn't my native language.
/Fredrik
Since every problem so far with my setup has been solved by reading old threads from this forum I thought my hopefully last but sadly most confusing problem could be solved here as well. My problem is that after I have connected with the MCU and try to debug I get this very informative error: 'No register.'
Edit: This always happens at 27% if that might be relevant.
I'm using the following setup:
Windows XP
Eclipse IDE helios (Build id: 20100917-0705)
OpenOCD 0.4.0
GNUARM
Cygwin
Olimex arm-usb-ocd
STR H711
When connecting I get this response:
Code: Select all
When building I get this text, this is the last and hopefully relevant part:
jtag_nsrst_delay: 500
jtag_ntrst_delay: 500
15 kHz
trst_and_srst srst_pulls_trst srst_gates_jtag trst_push_pull srst_open_drain
Warn : use 'str711.cpu' as target identifier, not '0'
Info : clock speed 15 kHz
Info : JTAG tap: str711.cpu tap/device found: 0x3f0f0f0f (mfg: 0x787, part: 0xf0f0, ver: 0x3)
Info : Embedded ICE version 1
Info : str711.cpu: hardware has 2 breakpoint/watchpoint units
Code: Select all
I don't know how to fix the main.sym error, I run this to complete the file:Linking: main.elf
arm-elf-gcc -mcpu=arm7tdmi -I. -gdwarf-2 -DROM_RUN -D__WinARM__ -D__WINARMSUBMDL_STR71x__ -O0 -Wall -Wcast-align -Wimplicit -Wpointer-arith -Wswitch -ffunction-sections -fdata-sections -Wredundant-decls -Wreturn-type -Wshadow -Wunused -Wa,-adhlns=src/vector.lst -I./include -I./str71x_lib/include -Wcast-qual -MD -MP -MF .dep/main.elf.d src/vector.o src/startup.o src/vectors.o src/main.o --output main.elf -nostartfiles -Wl,-Map=main.map,--cref,--gc-sections -lc -lm -lc -lgcc -L./str71x_lib -lSTR71x_lib -T./STR71x-ROM.ld
copying...
`cp main.elf main.out`
/cygdrive/c/GNUARM/bin/arm-elf-nm: 'a.out': No such file
Creating load file for Flash: main.hex
make: *** [main.sym] Error 1
arm-elf-objcopy -O ihex main.elf main.hex
Creating load file for Flash: main.bin
arm-elf-objcopy -O binary main.elf main.bin
Creating Symbol Table: main.sym
arm-elf-nm -n main.elf > main.sym
C:GNUARM\bin>arm-elf-nm.exe -n C:\projects\str_711\main.elf > C:\projects\str_711\main.sym
Here is the make file if anyone bothers to read it:
Code: Select all
I would be really happy if anyone could help me with this. I need this to work for a project at my new job, since everyone is on vacation I don't have anyone to ask for help...# Hey Emacs, this is a -*- makefile -*-
#
# WinARM template makefile
# by Giacomo Fazio and Antonio Nasca, Catania, Italy
# <giacomofazio@gmail.com>
# <antodani.nasca@hotmail.it>
#
# based on the WinARM template makefile written by Martin Thomas
# Released to the Public Domain
# Please read the make user manual!
#
#
# On command line:
#
# make all = Make software.
#
# make clean = Clean out built project files.
#
# make program = Download the hex file to the device
#
# (TODO: make filename.s = Just compile filename.c into the assembler code only)
#
# To rebuild project do "make clean" then "make all".
# Toolchain prefix (i.e arm-elf -> arm-elf-gcc.exe)
TCHAIN = arm-elf
#TCHAIN = arm-none-eabi
#USE_THUMB_MODE = YES
USE_THUMB_MODE = NO
# MCU name and submodel
MCU = arm7tdmi
SUBMDL = STR71x
## Create ROM-Image
RUN_MODE=ROM_RUN
## Create RAM-Image
#RUN_MODE=RAM_RUN
## not supported in this example:
## Exception-Vector placement only supported for "ROM_RUN"
## (placement settings ignored when using "RAM_RUN")
## - Exception vectors in ROM:
#VECTOR_LOCATION=VECTORS_IN_ROM
## - Exception vectors in RAM:
#VECTOR_LOCATION=VECTORS_IN_RAM
# Target file name (without extension).
TARGET = main
# List C source files here. (C dependencies are automatically generated.)
# use file-extension c for "c-only"-files
SRC = src/$(TARGET).c
# List C source files here which must be compiled in ARM-Mode.
# use file-extension c for "c-only"-files
SRCARM = src/vectors.c
# thumb is possible too for vectors.c - keep ARM, TODO: profile
# List C++ source files here.
# use file-extension cpp for C++-files (use extension .cpp)
CPPSRC =
# List C++ source files here which must be compiled in ARM-Mode.
# use file-extension cpp for C++-files (use extension .cpp)
#CPPSRCARM = $(TARGET).cpp
CPPSRCARM =
# List Assembler source files here.
# Make them always end in a capital .S. Files ending in a lowercase .s
# will not be considered source files but generated files (assembler
# output from the compiler), and will be deleted upon "make clean"!
# Even though the DOS/Win* filesystem matches both .s and .S the same,
# it will preserve the spelling of the filenames, and gcc itself does
# care about how the name is spelled on its command-line.
ASRC =
# List Assembler source files here which must be assembled in ARM-Mode..
ASRCARM = src/vector.S src/startup.S
# Path to Linker-Scripts
LINKERSCRIPTPATH = .
## Output format. (can be ihex or binary or both)
## (binary i.e. for openocd and SAM-BA, hex i.e. for lpc21isp and uVision)
#FORMAT = ihex
#FORMAT = binary
FORMAT = both
# Optimization level, can be [0, 1, 2, 3, s].
# 0 = turn off optimization. s = optimize for size.
# (Note: 3 is not always the best optimization level. See avr-libc FAQ.)
#OPT = s
OPT = 0
## Using the Atmel AT91_lib produces warning with
## the default warning-levels.
## yes - disable these warnings; no - keep default settings
#AT91LIBNOWARN = yes
AT91LIBNOWARN = no
# Debugging format.
# Native formats for AVR-GCC's -g are stabs [default], or dwarf-2.
# AVR (extended) COFF requires stabs, plus an avr-objcopy run.
#DEBUG = stabs
DEBUG = dwarf-2
# List any extra directories to look for include files here.
# Each directory must be seperated by a space.
EXTRAINCDIRS = ./include ./str71x_lib/include
# List any extra directories to look for library files here.
# Each directory must be seperated by a space.
#EXTRA_LIBDIRS = ../arm7_efsl_0_2_4
EXTRA_LIBDIRS = ./str71x_lib
# Compiler flag to set the C Standard level.
# c89 - "ANSI" C
# gnu89 - c89 plus GCC extensions
# c99 - ISO C99 standard (not yet fully implemented)
# gnu99 - c99 plus GCC extensions
CSTANDARD = -std=gnu99
# Place -D or -U options for C here
CDEFS = -D$(RUN_MODE)
# Place -I options here
CINCS =
# Place -D or -U options for ASM here
ADEFS = -D$(RUN_MODE)
ifdef VECTOR_LOCATION
CDEFS += -D$(VECTOR_LOCATION)
ADEFS += -D$(VECTOR_LOCATION)
endif
CDEFS += -D__WinARM__ -D__WINARMSUBMDL_$(SUBMDL)__
ADEFS += -D__WinARM__ -D__WINARMSUBMDL_$(SUBMDL)__
# Compiler flags.
ifeq ($(USE_THUMB_MODE),YES)
THUMB = -mthumb
THUMB_IW = -mthumb-interwork
else
THUMB =
THUMB_IW =
endif
# -g*: generate debugging information
# -O*: optimization level
# -f...: tuning, see GCC manual and avr-libc documentation
# -Wall...: warning level
# -Wa,...: tell GCC to pass this to the assembler.
# -adhlns...: create assembler listing
#
# Flags for C and C++ (arm-elf-gcc/arm-elf-g++)
CFLAGS = -g$(DEBUG)
CFLAGS += $(CDEFS) $(CINCS)
CFLAGS += -O$(OPT)
CFLAGS += -Wall -Wcast-align -Wimplicit
CFLAGS += -Wpointer-arith -Wswitch
CFLAGS += -ffunction-sections -fdata-sections
CFLAGS += -Wredundant-decls -Wreturn-type -Wshadow -Wunused
CFLAGS += -Wa,-adhlns=$(subst $(suffix $<),.lst,$<)
CFLAGS += $(patsubst %,-I%,$(EXTRAINCDIRS))
# flags only for C
CONLYFLAGS += -Wnested-externs
CONLYFLAGS += $(CSTANDARD)
ifneq ($(AT91LIBNOWARN),yes)
#AT91-lib warnings with:
CFLAGS += -Wcast-qual
CONLYFLAGS += -Wmissing-prototypes
CONLYFLAGS += -Wstrict-prototypes
CONLYFLAGS += -Wmissing-declarations
endif
# flags only for C++ (arm-elf-g++)
# CPPFLAGS = -fno-rtti -fno-exceptions
CPPFLAGS =
# Assembler flags.
# -Wa,...: tell GCC to pass this to the assembler.
# -ahlns: create listing
# -g$(DEBUG): have the assembler create line number information
ASFLAGS = $(ADEFS) -Wa,-adhlns=$(<:.S=.lst),-g$(DEBUG)
#Additional libraries.
# Extra libraries
# Each library-name must be seperated by a space.
# To add libxyz.a, libabc.a and libefsl.a:
# EXTRA_LIBS = xyz abc efsl
#EXTRA_LIBS = efsl
EXTRA_LIBS = STR71x_lib
#Support for newlibc-lpc (file: libnewlibc-lpc.a)
#NEWLIBLPC = -lnewlib-lpc
MATH_LIB = -lm
# CPLUSPLUS_LIB = -lstdc++
# Linker flags.
# -Wl,...: tell GCC to pass this to linker.
# -Map: create map file
# --cref: add cross reference to map file
LDFLAGS = -nostartfiles -Wl,-Map=$(TARGET).map,--cref,--gc-sections
LDFLAGS += -lc
LDFLAGS += $(NEWLIBLPC) $(MATH_LIB)
LDFLAGS += -lc -lgcc
LDFLAGS += $(CPLUSPLUS_LIB)
LDFLAGS += $(patsubst %,-L%,$(EXTRA_LIBDIRS))
LDFLAGS += $(patsubst %,-l%,$(EXTRA_LIBS))
# Set Linker-Script Depending On Selected Memory and Controller
ifeq ($(RUN_MODE),RAM_RUN)
LDFLAGS +=-T$(LINKERSCRIPTPATH)/$(SUBMDL)-RAM.ld
else
LDFLAGS +=-T$(LINKERSCRIPTPATH)/$(SUBMDL)-ROM.ld
endif
# Define directories, if needed.
## DIRARM = c:/WinARM/
## DIRARMBIN = $(DIRAVR)/bin/
## DIRAVRUTILS = $(DIRAVR)/utils/bin/
# Define programs and commands.
SHELL = sh
CC = $(TCHAIN)-gcc
CPP = $(TCHAIN)-g++
AR = $(TCHAIN)-ar
OBJCOPY = $(TCHAIN)-objcopy
OBJDUMP = $(TCHAIN)-objdump
SIZE = $(TCHAIN)-size
NM = $(TCHAIN)-nm
REMOVE = rm -f
REMOVEDIR = rm -f -r
COPY = cp
# Define Messages
# English
MSG_ERRORS_NONE = Errors: none
MSG_BEGIN = "-------- begin (mode: $(RUN_MODE)) --------"
MSG_END = -------- end --------
MSG_SIZE_BEFORE = Size before:
MSG_SIZE_AFTER = Size after:
MSG_FLASH = Creating load file for Flash:
MSG_EXTENDED_LISTING = Creating Extended Listing:
MSG_SYMBOL_TABLE = Creating Symbol Table:
MSG_LINKING = Linking:
MSG_COMPILING = Compiling C:
MSG_COMPILING_ARM = "Compiling C (ARM-only):"
MSG_COMPILINGCPP = Compiling C++:
MSG_COMPILINGCPP_ARM = "Compiling C++ (ARM-only):"
MSG_ASSEMBLING = Assembling:
MSG_ASSEMBLING_ARM = "Assembling (ARM-only):"
MSG_CLEANING = Cleaning project:
MSG_FORMATERROR = Can not handle output-format
MSG_LPC21_RESETREMINDER = You may have to bring the target in bootloader-mode now.
# Define all object files.
COBJ = $(SRC:.c=.o)
AOBJ = $(ASRC:.S=.o)
COBJARM = $(SRCARM:.c=.o)
AOBJARM = $(ASRCARM:.S=.o)
CPPOBJ = $(CPPSRC:.cpp=.o)
CPPOBJARM = $(CPPSRCARM:.cpp=.o)
# Define all listing files.
LST = $(ASRC:.S=.lst) $(ASRCARM:.S=.lst) $(SRC:.c=.lst) $(SRCARM:.c=.lst)
LST += $(CPPSRC:.cpp=.lst) $(CPPSRCARM:.cpp=.lst)
# Compiler flags to generate dependency files.
### GENDEPFLAGS = -Wp,-M,-MP,-MT,$(*F).o,-MF,.dep/$(@F).d
GENDEPFLAGS = -MD -MP -MF .dep/$(@F).d
# Combine all necessary flags and optional flags.
# Add target processor to flags.
ALL_CFLAGS = -mcpu=$(MCU) $(THUMB_IW) -I. $(CFLAGS) $(GENDEPFLAGS)
ALL_ASFLAGS = -mcpu=$(MCU) $(THUMB_IW) -I. -x assembler-with-cpp $(ASFLAGS)
# Default target.
all: begin gccversion sizebefore build sizeafter finished end
ifeq ($(FORMAT),ihex)
build: out elf hex lss sym
hex: $(TARGET).hex
IMGEXT=hex
else
ifeq ($(FORMAT),binary)
build: out elf bin lss sym
bin: $(TARGET).bin
IMGEXT=bin
else
ifeq ($(FORMAT),both)
build: out elf hex bin lss sym
hex: $(TARGET).hex
bin: $(TARGET).bin
else
$(error "$(MSG_FORMATERROR) $(FORMAT)")
endif
endif
endif
out: $(TARGET).out
elf: $(TARGET).elf
# lss: $(TARGET).lss
sym: $(TARGET).sym
# Eye candy.
begin:
@echo
@echo $(MSG_BEGIN)
finished:
@echo $(MSG_ERRORS_NONE)
end:
@echo $(MSG_END)
@echo
# Display size of file.
HEXSIZE = $(SIZE) --target=$(FORMAT) $(TARGET).hex
ELFSIZE = $(SIZE) -A $(TARGET).elf
sizebefore:
@if [ -f $(TARGET).elf ]; then echo; echo $(MSG_SIZE_BEFORE); $(ELFSIZE); echo; fi
sizeafter:
@if [ -f $(TARGET).elf ]; then echo; echo $(MSG_SIZE_AFTER); $(ELFSIZE); echo; fi
# Display compiler version information.
gccversion :
@$(CC) --version
# FLASH Programming with OPENOCD
# specify the directory where openocd executable resides (openocd-ftd2xx.exe or openocd-pp.exe)
# Note: you may have to adjust this if a newer version of YAGARTO has been downloaded
OPENOCD_DIR = 'C:\gccfd\openocd\bin'
# specify OpenOCD executable (pp is for the wiggler, ftd2xx is for the USB debugger)
#OPENOCD = $(OPENOCD_DIR)openocd-pp.exe
OPENOCD = openocd-ftd2xx.exe
# specify OpenOCD configuration file (pick the one for your device)
#OPENOCD_CFG = C:\openocd-configs\str71x-configs\str71x_signalyzer-flash-program.cfg
#OPENOCD_CFG = C:\openocd-configs\str71x-configs\str71x_jtagkey-flash-program.cfg
#OPENOCD_CFG = C:\openocd-configs\str71x-configs\str71x_armusbocd-flash-program.cfg
OPENOCD_CFG = armusbocd-flash-program.cfg
program:
@echo
@echo "Flash Programming with OpenOCD..."
$(OPENOCD) -f $(OPENOCD_CFG)
@echo
@echo
@echo "Flash Programming Finished."
# Create final output file (.out) from ELF output file.
%.out: %.elf
@echo "copying..."
`cp main.elf main.out`
# Create final output file (.hex) from ELF output file.
%.hex: %.elf
@echo
@echo $(MSG_FLASH) $@
$(OBJCOPY) -O ihex $< $@
# Create final output file (.bin) from ELF output file.
%.bin: %.elf
@echo
@echo $(MSG_FLASH) $@
$(OBJCOPY) -O binary $< $@
# Create extended listing file from ELF output file.
# testing: option -C
#%.lss: %.elf
# @echo
# @echo $(MSG_EXTENDED_LISTING) $@
# $(OBJDUMP) -h -S -C $< > $@
# Create a symbol table from ELF output file.
%.sym: %.elf
#%.sym:
@echo
@echo $(MSG_SYMBOL_TABLE) $@
$(NM) -n $< > $@
#%.elf:
# @echo
# @echo $(MSG_SYMBOL_TABLE) $@
# $(NM) -n main.elf > $@
# Link: create ELF output file from object files.
.SECONDARY : $(TARGET).elf
.PRECIOUS : $(AOBJARM) $(AOBJ) $(COBJARM) $(COBJ) $(CPPOBJ) $(CPPOBJARM)
%.elf: $(AOBJARM) $(AOBJ) $(COBJARM) $(COBJ) $(CPPOBJ) $(CPPOBJARM)
@echo
@echo $(MSG_LINKING) $@
$(CC) $(THUMB) $(ALL_CFLAGS) $(AOBJARM) $(AOBJ) $(COBJARM) $(COBJ) $(CPPOBJ) $(CPPOBJARM) --output $@ $(LDFLAGS)
# $(CPP) $(THUMB) $(ALL_CFLAGS) $(AOBJARM) $(AOBJ) $(COBJARM) $(COBJ) $(CPPOBJ) $(CPPOBJARM) --output $@ $(LDFLAGS)
# Compile: create object files from C source files. ARM/Thumb
$(COBJ) : %.o : %.c
@echo
@echo $(MSG_COMPILING) $<
$(CC) -c $(THUMB) $(ALL_CFLAGS) $(CONLYFLAGS) $< -o $@
# Compile: create object files from C source files. ARM-only
$(COBJARM) : %.o : %.c
@echo
@echo $(MSG_COMPILING_ARM) $<
$(CC) -c $(ALL_CFLAGS) $(CONLYFLAGS) $< -o $@
# Compile: create object files from C++ source files. ARM/Thumb
$(CPPOBJ) : %.o : %.cpp
@echo
@echo $(MSG_COMPILINGCPP) $<
$(CPP) -c $(THUMB) $(ALL_CFLAGS) $(CPPFLAGS) $< -o $@
# Compile: create object files from C++ source files. ARM-only
$(CPPOBJARM) : %.o : %.cpp
@echo
@echo $(MSG_COMPILINGCPP_ARM) $<
$(CPP) -c $(ALL_CFLAGS) $(CPPFLAGS) $< -o $@
# Compile: create assembler files from C source files. ARM/Thumb
## does not work - TODO - hints welcome
##$(COBJ) : %.s : %.c
## $(CC) $(THUMB) -S $(ALL_CFLAGS) $< -o $@
# Assemble: create object files from assembler source files. ARM/Thumb
$(AOBJ) : %.o : %.S
@echo
@echo $(MSG_ASSEMBLING) $<
$(CC) -c $(THUMB) $(ALL_ASFLAGS) $< -o $@
# Assemble: create object files from assembler source files. ARM-only
$(AOBJARM) : %.o : %.S
@echo
@echo $(MSG_ASSEMBLING_ARM) $<
$(CC) -c $(ALL_ASFLAGS) $< -o $@
# Target: clean project.
clean: begin clean_list finished end
clean_list :
@echo
@echo $(MSG_CLEANING)
$(REMOVE) $(TARGET).out
$(REMOVE) $(TARGET).hex
$(REMOVE) $(TARGET).bin
$(REMOVE) $(TARGET).obj
$(REMOVE) $(TARGET).elf
$(REMOVE) $(TARGET).map
$(REMOVE) $(TARGET).obj
$(REMOVE) $(TARGET).a90
$(REMOVE) $(TARGET).sym
$(REMOVE) $(TARGET).lnk
$(REMOVE) $(TARGET).lss
$(REMOVE) $(COBJ)
$(REMOVE) $(CPPOBJ)
$(REMOVE) $(AOBJ)
$(REMOVE) $(COBJARM)
$(REMOVE) $(CPPOBJARM)
$(REMOVE) $(AOBJARM)
$(REMOVE) $(LST)
$(REMOVE) $(SRC:.c=.s)
$(REMOVE) $(SRC:.c=.d)
$(REMOVE) $(SRCARM:.c=.s)
$(REMOVE) $(SRCARM:.c=.d)
$(REMOVE) $(CPPSRC:.cpp=.s)
$(REMOVE) $(CPPSRC:.cpp=.d)
$(REMOVE) $(CPPSRCARM:.cpp=.s)
$(REMOVE) $(CPPSRCARM:.cpp=.d)
$(REMOVEDIR) .dep | exit 0
# Include the dependency files.
-include $(shell mkdir .dep 2>/dev/null) $(wildcard .dep/*)
# Listing of phony targets.
.PHONY : all begin finish end sizebefore sizeafter gccversion \
build elf hex bin lss sym clean clean_list program
If there is any information that might be useful pleas let me know.
Pleas disregard the grammar errors, English isn't my native language.
/Fredrik