- Mon Jan 09, 2012 2:13 am
#137945
Hi, i managed to make a timer but my problem arises when i try to create an interrupt once the timer finishes. The timer works good. Here is the code:
Timer Initialization
Timer Initialization
Code: Select all
Interrupt
void init_timer (void)
{
VPBDIV = 0x1; //Set pclk to 19.6608 Mhz
T0PR = 0; //prescaler set to 0
T0TCR = 0x2; //Reset counter and prescaler
T0MCR = 0x3; //Reset on match. Interrupt Enabled
T0MR0 = 5000; //Set time
T0TCR = 0x1; //enable timer
VICVectAddr4 = (unsigned)T0isr; //Set the timer ISR vector address
VICVectCntl4 = 0x00000024; //Set channel
VICIntEnable |= 0x00000010; //Enable the interrupt
}
Code: Select all
Main
void T0isr (void) __irq
{
IOSET0 = 0x1; //Turn LED2 ON
Delay(); //Delay
IOCLR0 = 0x1; //Turn LED2 OFF
T0IR = 0x1; //Clear Match 0 interrupt
VICVectAddr = 0x00000000; //Dummy write to signal end of interrupt
}
Code: Select all
Thanks in advance.int main (void)
{
IODIR0 = 0xFFFFFFFF; //Set all pins as output
init_timer (); //Initialize timer
while(1)
{
IOSET0 = 0x2; //Turn LED1 ON
IOCLR0 = 0x2; //Turn LED1 OFF
}
}