- Wed Aug 03, 2011 7:10 am
#131262
I posted this on AVR freaks but I thought someone over here might know as well. Sorry to be "that guy"
I am trying to build a project for the Stellaris LM3S9B92 (EvalBot platform) with IAR EWARM 6.21.1.2846 and I don't seem to be getting the settings right. I have followed every relevant instructions I can find and don't see any differences between my set up and any of the example set ups.
Currently I'm getting a link error, or two rather but I'm guessing they are both arising from a single issue.
Error[Li005]: no definition for "__iar_program_start" [program entry]
Error[Li005]: no definition for "__iar_program_start" [referenced from C:\StellarisWare\boards\ek-lm3s9b92\bot_play\ewarm\Obj\startup_ewarm.o]
I have __iar_program_start defined as the entry symbol in my program just as the directions say. I only see that symbol used twice in any of the example projects. It's defined in the start up file and then placed at the reset vector in the vector table. Here is TI's startup_ewarm.c file
When I used to play with GCC and the AT91SAM7 chips you would see something like
Please help!
I am trying to build a project for the Stellaris LM3S9B92 (EvalBot platform) with IAR EWARM 6.21.1.2846 and I don't seem to be getting the settings right. I have followed every relevant instructions I can find and don't see any differences between my set up and any of the example set ups.
Currently I'm getting a link error, or two rather but I'm guessing they are both arising from a single issue.
Error[Li005]: no definition for "__iar_program_start" [program entry]
Error[Li005]: no definition for "__iar_program_start" [referenced from C:\StellarisWare\boards\ek-lm3s9b92\bot_play\ewarm\Obj\startup_ewarm.o]
I have __iar_program_start defined as the entry symbol in my program just as the directions say. I only see that symbol used twice in any of the example projects. It's defined in the start up file and then placed at the reset vector in the vector table. Here is TI's startup_ewarm.c file
Code: Select all
I have searched and searched and searched and I don't see __iar_program_start used anywhere else in any of the 20+ example projects. Google doesn't reveal much either. It's like the example programs just automagically jump to main from __iar_program_start.//*****************************************************************************
//
// startup_ewarm.c - Startup code for use with IAR's Embedded Workbench,
// version 5.
//
// Copyright (c) 2009-2011 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 6852 of the EK-LM3S9B92 Firmware Package.
//
//*****************************************************************************
//*****************************************************************************
//
// Enable the IAR extensions for this source file.
//
//*****************************************************************************
#pragma language=extended
//*****************************************************************************
//
// Forward declaration of the default fault handlers.
//
//*****************************************************************************
static void NmiSR(void);
static void FaultISR(void);
static void IntDefaultHandler(void);
//*****************************************************************************
//
// The entry point for the application startup code.
//
//*****************************************************************************
extern void __iar_program_start(void);
//*****************************************************************************
//
// Reserve space for the system stack.
//
//*****************************************************************************
static unsigned long pulStack[64] @ ".noinit";
//*****************************************************************************
//
// A union that describes the entries of the vector table. The union is needed
// since the first entry is the stack pointer and the remainder are function
// pointers.
//
//*****************************************************************************
typedef union
{
void (*pfnHandler)(void);
unsigned long ulPtr;
}
uVectorEntry;
//*****************************************************************************
//
// The vector table. Note that the proper constructs must be placed on this to
// ensure that it ends up at physical address 0x0000.0000.
//
//*****************************************************************************
__root const uVectorEntry __vector_table[] @ ".intvec" =
{
{ .ulPtr = (unsigned long)pulStack + sizeof(pulStack) },
// The initial stack pointer
__iar_program_start, // The reset handler
NmiSR, // The NMI handler
FaultISR, // The hard fault handler
IntDefaultHandler, // The MPU fault handler
IntDefaultHandler, // The bus fault handler
IntDefaultHandler, // The usage fault handler
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
IntDefaultHandler, // SVCall handler
IntDefaultHandler, // Debug monitor handler
0, // Reserved
IntDefaultHandler, // The PendSV handler
IntDefaultHandler, // The SysTick handler
IntDefaultHandler, // GPIO Port A
IntDefaultHandler, // GPIO Port B
IntDefaultHandler, // GPIO Port C
IntDefaultHandler, // GPIO Port D
IntDefaultHandler, // GPIO Port E
IntDefaultHandler, // UART0 Rx and Tx
IntDefaultHandler, // UART1 Rx and Tx
IntDefaultHandler, // SSI0 Rx and Tx
IntDefaultHandler, // I2C0 Master and Slave
IntDefaultHandler, // PWM Fault
IntDefaultHandler, // PWM Generator 0
IntDefaultHandler, // PWM Generator 1
IntDefaultHandler, // PWM Generator 2
IntDefaultHandler, // Quadrature Encoder 0
IntDefaultHandler, // ADC Sequence 0
IntDefaultHandler, // ADC Sequence 1
IntDefaultHandler, // ADC Sequence 2
IntDefaultHandler, // ADC Sequence 3
IntDefaultHandler, // Watchdog timer
IntDefaultHandler, // Timer 0 subtimer A
IntDefaultHandler, // Timer 0 subtimer B
IntDefaultHandler, // Timer 1 subtimer A
IntDefaultHandler, // Timer 1 subtimer B
IntDefaultHandler, // Timer 2 subtimer A
IntDefaultHandler, // Timer 2 subtimer B
IntDefaultHandler, // Analog Comparator 0
IntDefaultHandler, // Analog Comparator 1
IntDefaultHandler, // Analog Comparator 2
IntDefaultHandler, // System Control (PLL, OSC, BO)
IntDefaultHandler, // FLASH Control
IntDefaultHandler, // GPIO Port F
IntDefaultHandler, // GPIO Port G
IntDefaultHandler, // GPIO Port H
IntDefaultHandler, // UART2 Rx and Tx
IntDefaultHandler, // SSI1 Rx and Tx
IntDefaultHandler, // Timer 3 subtimer A
IntDefaultHandler, // Timer 3 subtimer B
IntDefaultHandler, // I2C1 Master and Slave
IntDefaultHandler, // Quadrature Encoder 1
IntDefaultHandler, // CAN0
IntDefaultHandler, // CAN1
IntDefaultHandler, // CAN2
IntDefaultHandler, // Ethernet
IntDefaultHandler, // Hibernate
IntDefaultHandler, // USB0
IntDefaultHandler, // PWM Generator 3
IntDefaultHandler, // uDMA Software Transfer
IntDefaultHandler, // uDMA Error
IntDefaultHandler, // ADC1 Sequence 0
IntDefaultHandler, // ADC1 Sequence 1
IntDefaultHandler, // ADC1 Sequence 2
IntDefaultHandler, // ADC1 Sequence 3
IntDefaultHandler, // I2S0
IntDefaultHandler, // External Bus Interface 0
IntDefaultHandler // GPIO Port J
};
//*****************************************************************************
//
// This is the code that gets called when the processor receives a NMI. This
// simply enters an infinite loop, preserving the system state for examination
// by a debugger.
//
//*****************************************************************************
static void
NmiSR(void)
{
//
// Enter an infinite loop.
//
while(1)
{
}
}
//*****************************************************************************
//
// This is the code that gets called when the processor receives a fault
// interrupt. This simply enters an infinite loop, preserving the system state
// for examination by a debugger.
//
//*****************************************************************************
static void
FaultISR(void)
{
//
// Enter an infinite loop.
//
while(1)
{
}
}
//*****************************************************************************
//
// This is the code that gets called when the processor receives an unexpected
// interrupt. This simply enters an infinite loop, preserving the system state
// for examination by a debugger.
//
//*****************************************************************************
static void
IntDefaultHandler(void)
{
//
// Go into an infinite loop.
//
while(1)
{
}
}
When I used to play with GCC and the AT91SAM7 chips you would see something like
Code: Select all
but I don't see anything like that in any of the working examples. Just on a slightly educated hunch I renamed my main function from main() to __iar_program_start and I was successfully able to build and load code onto my hardware. The debugger complained when it couldn't find main but I told it to shut up and it jumped right to __iar_program_start and then let me single step through the code. I turned some LED's on just to make sure it was in fact running.void __iar_program_start()
{
low_level_init();
main();
}
Please help!