- Mon Aug 01, 2011 12:32 am
#131089
Hello,
I am using a SAM9-L9260. I tried to boot it using the procedure described under:
The only thing I get on the HyperTerminal is ">romBOOT"
What am i doing wrong?
I am using a SAM9-L9260. I tried to boot it using the procedure described under:
SOFTWARE development with SAM9-L9260:
Overview
The board comes with Linux preloaded in the NAND flash. It's based on a
custom-built kernel and a Debian 4.0 userland. To use it, connect a nullmodem
cable to the board and to a serial port on your computer, start a
terminal program (e.g. HyperTerminal on Windows, minicom on Unix
systems) and configure it to use a 115200 baud rate, 8 data bist, 1 stop bit
and no parity and no flow control. Then apply power to the board (use a
5VDC regulated power supply with at least 500mA output current) and
you should see the board start-up messages.
The only thing I get on the HyperTerminal is ">romBOOT"
What am i doing wrong?