- Fri Mar 31, 2006 3:03 am
#11721
I'm hoping to be able to write a .hex to the flash of the LPC-H2148 through the usb port on the board, with an open source version of LPC2000 ISP, (lpc21isp). The problem is that the small lpc2148 header board doesn't have the boot loader pins broken out.
After reading Jim Lynch's tutorial ( http://www.olimex.com/dev/pdf/ARM%20Cro ... on%203.pdf ) and this thread ( http://www.sparkfun.com/cgi-bin/phpbb/v ... php?t=2582 ) , It seems like even with those pins broken out, since the lpc2148's usb port is not serial converted to usb via an ftdi chip (or whatever usb->serial bridge), I can't use the lpc21isp program. Is that right? If I plug the header board into the usb port, then pull down p0.14, hit reset then then undo p0.14 will that load the boot-loader and allow the LPC2000 ISP program to upload a .hex?
If not, is there any other way to upload code to the LPC-H2148 header board via usb?
Thank you for reading.
Tom
After reading Jim Lynch's tutorial ( http://www.olimex.com/dev/pdf/ARM%20Cro ... on%203.pdf ) and this thread ( http://www.sparkfun.com/cgi-bin/phpbb/v ... php?t=2582 ) , It seems like even with those pins broken out, since the lpc2148's usb port is not serial converted to usb via an ftdi chip (or whatever usb->serial bridge), I can't use the lpc21isp program. Is that right? If I plug the header board into the usb port, then pull down p0.14, hit reset then then undo p0.14 will that load the boot-loader and allow the LPC2000 ISP program to upload a .hex?
If not, is there any other way to upload code to the LPC-H2148 header board via usb?
Thank you for reading.
Tom