- Sat Feb 05, 2011 9:29 am
#119341
Well, I am just wondering... I have seen like 5 schematics and all of them have VREF connected to the power supply... and about the same for VBAT... also, are these(the pins that you suggested me to connect to JTAG aren't the only ones I see on other schematics) the only ones I need to connect to jtag to program the processor properly? Do I need a reset circuit(rst is connected to jtag though)? Why are the jtag pull ups resistors used in the schematics I see while in the jtag application note there are no pull ups used(It mentions though that the resistors should be used if the distance between the core and the jtag is bigger than 5cm and it isn't in most of the boards.), all the boards I saw were from Olimex, micro4you and some boards from the lpc2000 family, the lpc2000 yahoo group files and also some others that I came up googling