Hi
If the binary is running you should see LCD back-light blinking.
Remove the USB cable and connect again. When the USB cable is connected to the operating board with inserted SD card, the SD card will appear as a disk drive to the PC.
You can also connect to the board via TELNET at 192.168.0.3 or via the serial port (115kBaud). Once connected there are menus to change the IP settings if required.
The following tutorial also guides to loading web pages and using the web browser:
http://www.utasker.com/docs/SAM7X/uTaskerV1-4_SAM7X.PDF.
When connected via TELNET or UART you will see messages informing whether the SD card was detected of not. If no SD card is found it will try approx. ever 15s to see whether one has been inserted in the meantime. Assuming that it detected an SD card (SD or HCSD - not MMCs) you can then use the DOS-like menu interface to look at the directories and files, create, rename, etc. according to
http://www.utasker.com/docs/uTasker/uTasker_utFAT.PDF
Furthermore it is possible to copy large web sites to the SD card and the web browser on the board will serve these. The SD card is also visible via FTP.
If you can get the SD card to be detected it will verify that your board is working correctly with the interface and give you a reference as to what the SPI signals between the SD card and the ATMEL device do.
Good luck
Regards
Mark
www.uTasker.com