Page 1 of 1
lpc2148
Posted: Fri Nov 13, 2009 4:38 am
by naz
Hello All,
i'm struggling to receive data from gps receiver module to terminal window using lpc2148 in keiluvision 4 .i'm getting some junk data on terminal window.my baud rate is correct,i tried so many ways but i couldn't catch the error.Any one give some idea to solve this issue.
Re: lpc2148
Posted: Fri Nov 13, 2009 1:06 pm
by stevech
naz wrote:Hello All,
i'm struggling to receive data from gps receiver module to terminal window using lpc2148 in keiluvision 4 .i'm getting some junk data on terminal window.my baud rate is correct,i tried so many ways but i couldn't catch the error.Any one give some idea to solve this issue.
well, you've given us no specific symptoms. I have received 4800baud NMEA sentences on an LPC2106. Do you have the serial data voltage levels and data polarity correct?
Posted: Fri Nov 13, 2009 3:43 pm
by Shifted
Your baud rate might be correct, but are your clocks set up correctly?
Can you use a different device to input correct data to the processor (like a computer)?
Can you post any code from your MCU setup routines?
Posted: Fri Nov 13, 2009 4:59 pm
by leon_heller
Transmit 'U' continuously and use a scope to check the baud rate.
Leon
Posted: Fri Nov 13, 2009 11:38 pm
by naz
this is the code which i have tried.could u please tell where i'm doing the mistake
[color=green][code]#include<LPC214x.h>
#include<stdio.h>
void led(int);
void wait(void);
void serial(void);
char sendchar(char ch);
char recechar(void);
void __irq FIQ_Handler(void);
int main()
{
int ch;
IODIR1=0x00FF0000;
serial();
led(16);
EXTMODE |=0x02;//level sensitivity for EINT1
EXTPOLAR |=0x02;//polartiy for EINT1
PINSEL0|=0x20000000; //GPIO0.14,EINT1
EXTINT =0x00000002; //clear EINT flag register
VICIntEnable=0x00008000;
VICIntEnable=0x00008000; //enable interrupt 15
while(1)
{
recechar();
led(17);
ch=U1RBR;
sendchar(ch);
led(18);
}
}
void serial()
{
PINSEL0=0xFFF0FFFF; //clear uart1
PINSEL0|=0x00050000;//TX,RX of uart1
U1LCR =0x83;//8bit,no parity,1stop bit,enable DLAB
U1DLM =0x01;
U1DLL=0x87;
U1LCR&=0x7F; //disable DLAB
U1IER = 0x07; //enable interrrupt
}
char sendchar(char ch)
{
if(ch=='\n')
{
while(!(U1LSR&0x20));
U1THR=0x0D;
}
while(!(U1LSR&0x20));
return(U1THR);
}
char recechar()
{
while(!(U1LSR&0x01));
if(U1RBR=='$')
led(23);
return(U1RBR);
}
void led(int n)
{
IOSET1|=1<<n;
wait();
IOCLR1|=1<<n;
wait();
}
void wait()
{
int i;
for(i=0;i<8000000;i++);
}
void __irq FIQ_Handler()
{
EXTINT&=0x00000002; //disable interrupt.
}[/color][/code][/quote]
Posted: Sat Nov 14, 2009 7:48 am
by leon_heller
Here is some UART code I use:
Code: Select all//------------------------ UART1 ISR ------------------------//
static void uart1ISR(void)
{
/* Read IIR to clear interrupt and find out the cause */
unsigned iir = U1IIR;
/* Handle UART1 interrupt */
switch ((iir >> 1) & 0x7)
{
case 1:
/* THRE interrupt */
break;
case 2:
/* RDA interrupt */
do
{
uint16_t temp;
// calc next insert index & store character
temp = (uart1_rx_insert_idx + 1) % UART1_RX_BUFFER_SIZE;
uart1_rx_buffer[uart1_rx_insert_idx] = U1RBR;
// check for more room in queue
if (temp != uart1_rx_extract_idx)
uart1_rx_insert_idx = temp; // update insert index
}
while (U1LSR & 0x01);
break;
case 3:
/* RLS interrupt */
break;
case 6:
/* CTI interrupt */
break;
}
}
/* Description:
* This function gets a character from the UART1 receive queue
*
* Calling Sequence:
* void
*
* Returns:
* character on success, -1 if no character is available
*
*****************************************************************************/
int uart1Getch(void)
{
uint8_t ch;
if (uart1_rx_insert_idx == uart1_rx_extract_idx) // check if character is available
return -1;
ch = uart1_rx_buffer[uart1_rx_extract_idx++]; // get character, bump pointer
uart1_rx_extract_idx %= UART1_RX_BUFFER_SIZE; // limit the pointer
return ch;
}
//put this in the init. function
// initialise PLL
PLL0CFG=0x24; // Cclk = 60Mhz
PLL0CON=0x01;
PLL0FEED=0xAA;
PLL0FEED=0x55;
while(!(PLL0STAT & 0x0400))
;
PLL0CON=0x3;
PLL0FEED=0xAA;
PLL0FEED=0x55;
// initialise MAM and VPB
MAMTIM=0x3; // 3 cycles to read from FLASH
MAMCR=0x2; // MAM functions fully enabled
APBDIV=0x02; // Pclk = 30MHz
// initialise pclk (30 MHz)
unsigned long pclk = liblpc2000_get_pclk(liblpc2000_get_cclk(OSCILLATOR_CLOCK_FREQUENCY));
// initialise UART1 (RxD1 P0.9, TxD1 P0.8
U1LCR = 0x83; // 8 bit, 1 stop bit, no parity, enable DLAB
U1DLL = 0xC3; // set for 9600 baud
U1DLM = 0x00;
U1LCR &= ~0x80; // disable DLAB
U1FCR = 1; // enable FIFO
PINSEL0 = PINSEL0 & ~(0xFFFF << 16) | (0x5555 << 16);
// initialise Rx circular buffer
uart1_rx_extract_idx = uart1_rx_insert_idx = 0;
You probably don't need the circular buffer, so you can remove the relevant code.
Leon