SparkFun Forums 

Where electronics enthusiasts find answers.

Everything ARM and LPC
By mrick0363
#78142
Hello,
i just receive a LPC2478-STK evaluation board from OLIMEX and i would like to flash U-BOOT on it with Flash Magic (for testing flashing procedure) but i can't because i always have "Failed to autobaud - step 1". I have configure ,


Step 1 as :

Device : LPC2478
COM Port : COM 1 (real com port from PC, not FTDI)
Baud rate : 9600
Interface : None (ISP)
Oscillator (MHz) : 12

Step 2 as :
tick "Erase all Flash+Code Rd Prot"

Step 3 Hex File from correct location

Step 4 : None tick


I can't go to flash magic forum because of my enterprise internet restriction (it sucks !, sorry).

Then can anyone help me to find correct procedure ?
Thanks a lot

PS : In normal operation ,the board boot correctly ,i see penguin on LCD and text on PC COM1 terminal , i can entering into UBOOT menu or let uclinux boot on USB mass storage
By mrick0363
#78286
Hello,
finally it simply the null modem cable which was defect (Pin6 connect to Pin8).Now it's ok.
By king_8210
#78297
So...your problem was that the null modem cable was defect ?

And then you changed another one , now it's ok ?

I have the same problem with you .

But I can't find the solution .

You can say it more detailed ?

Thank you for grateful .