SparkFun Forums 

Where electronics enthusiasts find answers.

Questions &/or issues related to products in the Miscellaneous category should be posted in this forum. For Kits, please post in the Kits forum.
#205751
I'm prototyping a sound level meter for a physics experiment. I teach physics at a small college. I'm using the uLCD-32PTU-AR to display a meter to show max sound amplitude (using microphone breakout) and led digits to show ADC sample rate.

I am finding that if I use a Blackboard, the meter doesn't work but the led digits do! When I use an Arduino Uno the display responds as expected.

Since the Blackboard is supposed to be compatible with the Uno, what could be going on?

I've attached a picture of my setup, my sketch, and the resource files for the display.

Thanks!
You do not have the required permissions to view the files attached to this post.
#205759
Do you have a link to that shield, LCD screen, and microphone(?) (I don't think we carry some of those products)? Could the selectable I/O voltage be causing an issue?

When you say, "the meter doesn't work but the led digits do," are you referring to the green digits on the LCD screen?

Have you tried to debug the code to see if you are getting proper values for the meter? Try a simple Serial.print() function to output that value.
  1. Do the values look right?
  2. If there is no response, try to check your wiring to the analog pin.
  3. Try testing the analog pin with a simple analogread sketch and trimpot.
#205765
I bought all the parts from SparkFun - the 4d display shield for Arduino Uno (the red thing on top of my Arduino), the 4d display (the thing in foreground), the microphone breakout (the red thing in background on the breadboard).

If you look at my sketch, I have a "Serial.println(meterVal)" which I can compile back in by changing the "#if 0" to "#if 1". The values on the serial monitor in this case are what I expect.

If I swap out the Arduino for the Blackboard (also from Sparkfun), the readings on the LED digits (on the LCD screen) are correct and update with each loop(). However, the meter on the display is stuck at 50 and does not respond, despite my whistling or clapping. Swap back in the Arduino and I'm back in business.

I'm not sure I fathom what you mean by "selectable I/O voltage" causing an issue. The Blackboard is unaltered as received from SparkFun.

I uploaded my sketch and the resource files to my original post. I was hoping someone at SparkFun could replicate the setup and confirm Blackboard doesn't update the meter object for some reason. The components and part numbers are:

* Microphone breakout INMP401 (ADMP401) part BOB-09868:
* VCC -> 3.3V,
* GND -> GND,
* VOUT -> A0
* uLCD-32PTU-AR part LCD-11741 (comes with shield and cable), USB-to-Serial Bridge uUSB-PA5-II part DEV-15009 for programming display with 4D Workshop
* Blackboard C part SPX-15098
* using the genieArduino library in my sketch
#205767
An update ... I set up a simple circuit with Blackboard and a potentiometer and wrote a small sketch to print out A0 every 0.5 seconds. Naturally, it works fine (see attached photo). The trace is serial plotter and me playing with potentiometer and A0 gives values from 0 to 1023.
Capture.PNG
I then put the 4D shield for Arduino (comes in the uLCD box along with the display and cable) and repeated the test with potentiometer. I got a similar plot with values ranging from 0 to 1023.

I believe this is pointing towards something in my sketch which gives different behavior depending on whether I'm putting the sketch on Ardunio Uno or Blackboard. So I will experiment with my sketch.
You do not have the required permissions to view the files attached to this post.
#205840
YEAH! I have narrowed down the issue to the 4d-Arduino-Display adapter (the red shield that came with the display).

If I change jumpers J3 and J4 on that adapter to use D2 and D3 for RX and TX, and use SoftwareSerial in my sketch, everything works!

The documentation for the adapter says it works with "most" Arduinos, but until I changed J3 and J4 it wouldn't work.

Hope this helps someone else.