SparkFun Forums 

Where electronics enthusiasts find answers.

Search found 367 matches

 Go to advanced search

 by OLIMEX ¦  Fri Aug 17, 2007 7:24 am ¦  Forum: Everything ARM and LPC ¦  Topic: Problem with LCD (GE8) on SAM7-EX256 ¦  Replies: 5 ¦  Views: 2225

GE8 doesn't support 8-bit mode
Best regards
Tsvetan

 by OLIMEX ¦  Fri Aug 03, 2007 3:50 am ¦  Forum: Everything ARM and LPC ¦  Topic: CS-E9302 board, boot problem ¦  Replies: 1 ¦  Views: 1066

5V 1A adapter should be used
Tsvetan

 by OLIMEX ¦  Tue Jul 24, 2007 1:59 am ¦  Forum: MSP Microcontrollers ¦  Topic: Olimex JTAG-TINY + MSPGCC ¦  Replies: 7 ¦  Views: 4923

hi,
several customers of ours reported that they use Tiny and Iso with MSPGCC but we never try, you can ask on MSPGCC list or look at this list archives there should be postings how to set the enviroment
Best regards
Tsvetan

 by OLIMEX ¦  Mon Jul 23, 2007 3:53 am ¦  Forum: Everything ARM and LPC ¦  Topic: lib-lpc2k - new open-source hardware library for LPC2xxx ¦  Replies: 2 ¦  Views: 1424

this is very good idea.
we are going to re-arrange the examples on our web in the next few weeks, but you can use all our web software examples if you find them useful
Tsvetan

 by OLIMEX ¦  Fri Jul 20, 2007 8:51 am ¦  Forum: Everything ARM and LPC ¦  Topic: I want them all! Help me choose my next ARM7 board ¦  Replies: 8 ¦  Views: 2390

leon_heller wrote:The quality is better, and the proto board is very comprehensive.

Leon
this is very comprehensive answer, I can't see you in our database to have purchased anything than MSP430-JTAG-TINY, so how do you judge our LPC boards quality?

Best regards
Tsvetan

 by OLIMEX ¦  Thu Jul 19, 2007 9:33 am ¦  Forum: OpenOCD ¦  Topic: ARM-USB-TINY shipped Windows USB drivers have wrong PID ¦  Replies: 2 ¦  Views: 1808

if you install the software which comes with the CD this is very unlickely to happend
the software on CD have descriptions for both ARM-USB-OCD and ARM-USB-TINY and windows will install the drivers without any "manual" work

Best regards
Tsvetan

 by OLIMEX ¦  Sun Jul 15, 2007 5:17 am ¦  Forum: MSP Microcontrollers ¦  Topic: Newbie / JTAG-TINY to USB with IAR embedded workbench ¦  Replies: 1 ¦  Views: 1402

why don't you read what to do from the how to install .txt in our MSP430-JTAG-TINY zip with the drivers?
tip: the new EW-MSP430 have Olimex JTAG option to select.
otherwise on the old EW-MSP430 you have to use TI USB-FET as written on our web

Best regards
Tsvetan

 by OLIMEX ¦  Wed Jul 11, 2007 12:04 am ¦  Forum: AVR Microcontrollers ¦  Topic: AVR-IO-M16 Input question ¦  Replies: 6 ¦  Views: 4215

1) correct to read the input make sure you do this: - supply voltage with enough current capability to light on 2 LEDs i.e. 10mA, also make sure voltage is 5V or above as the voltage drop on the LEDs alone is 2+2 V - you supply the voltage with correct polarity , if your input LED is ON this means y...

 by OLIMEX ¦  Fri Jul 06, 2007 2:13 am ¦  Forum: Everything ARM and LPC ¦  Topic: Olimex 2378 dev board software ¦  Replies: 7 ¦  Views: 2627

e-mail where you have bought the boards and ask for the code?
definitely here is not the place where you will receive copyrighted code
Tsvetan

 by OLIMEX ¦  Tue Jul 03, 2007 7:06 am ¦  Forum: OpenOCD ¦  Topic: ST's STFM32 range of micros ¦  Replies: 8 ¦  Views: 3562

we have 3 STM32 development boards with prices in range $33-$80
the information will be uploaded this week on our web.
STM32 devices will be in range of $3-$4 for 1K order
ST will start shipping them in September this year

 by OLIMEX ¦  Mon Jul 02, 2007 3:36 am ¦  Forum: Everything ARM and LPC ¦  Topic: Any interest in .NET Micro Framework? ¦  Replies: 4 ¦  Views: 1548

correct me if I'm wrong, but for embedded system 300K just to say "hello world" is quite waste of resources

Tsvetan

 by OLIMEX ¦  Mon Jul 02, 2007 3:34 am ¦  Forum: Everything ARM and LPC ¦  Topic: New PHY driver in EP9302 board ¦  Replies: 1 ¦  Views: 899

every board comes with CD and there are applied the necessary patches to work with the PHY on board

Tsvetan

 by OLIMEX ¦  Fri Jun 29, 2007 5:25 am ¦  Forum: Everything ARM and LPC ¦  Topic: Olimex 2378 dev board software ¦  Replies: 7 ¦  Views: 2627

Hi,
did you got our e-mail yesterday?
Tsvetan

 by OLIMEX ¦  Thu Jun 28, 2007 10:24 pm ¦  Forum: Everything ARM and LPC ¦  Topic: Olimex 2378 dev board software ¦  Replies: 7 ¦  Views: 2627

you will receive this software from the place you bought the board
Best regards
Tsvetan

 by OLIMEX ¦  Thu Jun 28, 2007 12:22 am ¦  Forum: AVR Microcontrollers ¦  Topic: Mega2560 development boards ¦  Replies: 2 ¦  Views: 1308

hi, we restrain and release boards only for AVRs which are supported by our JTAGs no much sense to offer board which is not supported by your JTAG tools as there would be tons of questions - why I can\t use your JTAGs to work with your boards ;) Atmel have some weird policy to offer several tools wh...

  • 1
  • 2
  • 3
  • 4
  • 5
  • 25