SparkFun Forums 

Where electronics enthusiasts find answers.

Search found 215 matches

 Go to advanced search

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Mon Apr 16, 2012 9:53 am ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

I'm working right now to get the display to read the serial line and display the data. I'm having a fair amount of difficulty with that, even though it should be a pretty easy program. Once I can read and display the serial data consistently, I'll have the display working very quickly. I just keep b...

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Mon Apr 16, 2012 7:57 am ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

I'm working on getting better information about interrupts (Dan, I hate to keep pestering you about it, but you're a guru in this area).
I need to leave digital pins two and three free for interrupts, correct?

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Mon Apr 16, 2012 7:37 am ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

Sorry about the lack of posts. I've been puzzling the serial sending and receiving without huge success (but some small minor successes). Also, it looks like I'm going back to real work (Another 6 hours of waiting to see if everything is holding together). Is there any kind of timing disadvantage to...

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Sun Apr 08, 2012 6:58 am ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

Get yours done!

I'm waiting for some IR LEDs to come in, and then I'm going to play with beam forming in the basement

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Sat Apr 07, 2012 12:48 pm ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

I don't think it's that smart... When I first started playing with it, I had issues with programming the Arduino with the display attached. I think I may have to get a DPDT switch, something that disconnects the display when the USB connection needs to be active. That will solve a lot of problems an...

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Sat Apr 07, 2012 8:47 am ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

When I first went back to this project, in December or January, I looked at using Avenue33's code. There were a couple of issues. First, his library hadn't been updated for use with Arduino 1.0, and required a hodge-podge of NewSoftSerial and some modification of other libraries. I couldn't get thin...

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Fri Apr 06, 2012 6:06 pm ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

Alright, I think we're at the next stage. I need to figure out the serial communication between the Arduino and the uOLED. I'm not completely sure how serial communications work, so I'm going to talk out loud. I think both systems are capable of communicating at 57600 (56K) baud. Baud refers to the ...

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Fri Apr 06, 2012 7:42 am ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

Yep. I can't rave about this screen enough (except for the learning curve, the price you pay for an insane number of options). http://www.4dsystems.com.au/prod.php?id=85 OLED display Able to be driven either through an onboard microprocessor (taking information from onboard I/O pins and serial) or d...

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Fri Apr 06, 2012 7:28 am ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

Have fun on vacation! I'm playing with the display this week. I think I found what my problem was. It's going to be a bit of an uphill battle for me. The display uses a different language for programming. It's not rocket science, once I get beyond the serial commands. It would probably help if I had...

Re: ATMega Lasertag

 by StaticDet5 ¦  Thu Apr 05, 2012 9:23 am ¦  Forum: SparkFun Product Questions ¦  Topic: ATMega Lasertag ¦  Replies: 36 ¦  Views: 5488

I had a friend over the other day, and his big questions were about beam size and forming (Forget my project. He "hrmph'd" over it, and that was that). He asked some real pointed questions (that I probably should have been able to answer, but I'm not real sure about the practical applications of the...

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Thu Apr 05, 2012 7:35 am ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

In that vein, I'm updating the "To-Do" list, before I can think about making the PCB backpack: 1. Low Battery Cut-Out 2. Thermal Monitoring 3. Selector Switch (I have a cool part for this, but it's very limited) 4. Pin Breakout and Allocation (There are certain pins that are going to be common to ev...

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Wed Apr 04, 2012 1:32 pm ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

That's what I'm hoping for. For the "benchtop" testing, I'm just going to wire up a push-button. Again, the problem with the AEG's is that each model is different. The P90, AR-series, etc, all have different mechanisms for selecting the fire mode. Also, this system potentially allows for more fire m...

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Wed Apr 04, 2012 9:14 am ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

/* GearboxParkingUsingADC 4-3-2012 previous working code BasicAirsoftBarrelSensor The circuit: * LED on board at pin 13 * Motor control on pin 3 (PWM pin) * pushbutton attached to pin 7 from +5V * 10K resistor attached to pin 7 from ground * ADC on analog pin 0 * The photo-interrupter on pin 2 Seri...

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Tue Apr 03, 2012 5:25 pm ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

The code needs some tweaking, but the basic fire control coding is done. Safe, Semi, Burst, Full is all working, though there are some occasional "extra-fires". I'll post some code in the morning.

Re: Arduino Airsoft Controller with Display

 by StaticDet5 ¦  Tue Apr 03, 2012 7:34 am ¦  Forum: SparkFun Product Questions ¦  Topic: Arduino Airsoft Controller with Display ¦  Replies: 465 ¦  Views: 56139

/* GearboxParkingUsingADC 4-3-2012 previous working code BasicAirsoftBarrelSensor The circuit: * LED on board at pin 13 * Motor control on pin 3 (PWM pin) * pushbutton attached to pin 7 from +5V * 10K resistor attached to pin 7 from ground * ADC on analog pin 0 * The photo-interrupter on pin 2 Seri...

  • 1
  • 2
  • 3
  • 4
  • 5
  • 15