SparkFun Forums 

Where electronics enthusiasts find answers.

Search found 6 matches

 Go to advanced search

Re: Tsunami loop stop

 by klippard ¦  Sun Dec 31, 2017 1:16 pm ¦  Forum: SparkFun Product Questions ¦  Topic: Tsunami loop stop ¦  Replies: 8 ¦  Views: 372

Works perfectly with the new mono firmware! Exactly what I needed! Thanks very much for the update! I'll give it a try with the stereo firmware as well and report back.

Re: Tsunami loop stop

 by klippard ¦  Sat Dec 30, 2017 9:00 pm ¦  Forum: SparkFun Product Questions ¦  Topic: Tsunami loop stop ¦  Replies: 8 ¦  Views: 372

I do wish the polyphonic option worked a bit different in this situation though. Without it, every time I switch between looping tracks, it interrupts normal tracks that may be playing via other triggers. If I turn on the polyphonic option for the looping tracks, both tracks start playing on top of ...

Re: Tsunami loop stop

 by klippard ¦  Sat Dec 30, 2017 7:56 pm ¦  Forum: SparkFun Product Questions ¦  Topic: Tsunami loop stop ¦  Replies: 8 ¦  Views: 372

I was using the 1.04 stereo firmware and the Unified 2.0 Configurator. I re-created a new .ini file with the 0.31 configurator, but that still did not work. I did have polyphonic checked, but even unchecking that didn't seem to make any difference. I then flashed the Tsunami with the mono firmware, ...

Re: Tsunami loop stop

 by klippard ¦  Sat Dec 30, 2017 3:29 pm ¦  Forum: SparkFun Product Questions ¦  Topic: Tsunami loop stop ¦  Replies: 8 ¦  Views: 372

Thanks for your reply! The stop function is certainly an option, but I don't want to waste a trigger input on that if I don't have to. The trigger type is set to "edge" and the function is set to "next". If I uncheck "loop" the next function does indeed work properly and the board plays the next tra...

Re: Tsunami loop stop

 by klippard ¦  Sat Dec 30, 2017 9:01 am ¦  Forum: SparkFun Product Questions ¦  Topic: Tsunami loop stop ¦  Replies: 8 ¦  Views: 372

What I am really looking for here is a way to switch between two different looping tracks using a single trigger. I thought I had found a way to do it using the NEXT function with the loop option checked and track range set between 2 tracks, but it is not working. When the trigger is activated, it s...

Tsunami loop stop

 by klippard ¦  Fri Dec 29, 2017 6:46 am ¦  Forum: SparkFun Product Questions ¦  Topic: Tsunami loop stop ¦  Replies: 8 ¦  Views: 372

Short of a system reset, is there a way to stop an automatic looping track once it starts on the Tsunami board? I've tried setting the trigger to level and holding it low to loop, but the looping is not as smooth that way as it is with automatic looping. What I am really looking for is a feature to ...