Search found 55 matches

by exeng
Thu Oct 11, 2018 5:56 pm
Forum: Projects
Topic: Alternating 3 LED project
Replies: 3
Views: 200

Re: Alternating 3 LED project

Following up on my previous post... also look at figure 11 where reset is used to sequence only a subset of the 10 outputs. In your case 3 for equal on times.
by exeng
Thu Oct 11, 2018 5:29 pm
Forum: Projects
Topic: Alternating 3 LED project
Replies: 3
Views: 200

Re: Alternating 3 LED project

Seems to me that you could adapt a simple circuit like this (see figures 6-7) here-> http://www.nutsvolts.com/magazine/article/led-chaser-sequencer-circuits without using a micro. Simply connect the GRN led to outputs 0-3, YEL led to 4-5, and RED led to 6-9 (or some combination that results in the r...
by exeng
Tue May 29, 2018 7:20 pm
Forum: Arduino
Topic: WiFi robot project, help with shopping list and guidance
Replies: 3
Views: 319

Re: WiFi robot project, help with shopping list and guidance

Have you seen the WiFi controlled robot tutorial by Alex the Giant of Sparkfun fame?

Here is a link to the tutorial: https://learn.sparkfun.com/tutorials/wi ... 1504673727
by exeng
Fri May 11, 2018 9:24 am
Forum: SparkFun Product Questions
Topic: Tsunami firmware update problem.
Replies: 7
Views: 350

Re: Tsunami firmware update problem (PIR motion tip).

I've used a PIR motion sensor with the WAV Trigger board controlled by a Mega (Uno would work too). One of the things I ran into was an annoying re-trigger behavior of the PIR sensor. As a result I ended up using a version of this code (https://playground.arduino.cc/Code/PIRsense) which forces a del...
by exeng
Sat Apr 14, 2018 9:01 am
Forum: SparkFun Product Questions
Topic: MP3 Trigger Micro sd card
Replies: 1
Views: 165

Re: MP3 Trigger Micro sd card

From the MP3 Trigger Hookup Guide on the Sparkfun site...
Basic Operation
Simply drag and drop the desired MP3 files into the root directory of a FAT32 or FAT16 formatted microSD flash card using a PC.
Root directory.
by exeng
Fri Mar 30, 2018 11:11 pm
Forum: SparkFun Product Questions
Topic: Wav Trigger Serial control with arduino nOOb question
Replies: 5
Views: 351

Re: Wav Trigger Serial control with arduino nOOb question

On the Mega I use AltSoftSerial to control the WAV Trigger serially as follows... #include <AltSoftSerial.h> // AltSoftSerial uses Arduino Mega 2560 pins 48 RX and 46 TX connected the the WAV Trigger TX and RX respectively. Not sure what else you are looking for exactly beyond the example sketch for...
by exeng
Tue Feb 06, 2018 10:01 am
Forum: SparkFun Product Questions
Topic: WAV Trigger voltage signal
Replies: 10
Views: 436

Re: WAV Trigger voltage signal

Perhaps you can share a bit more about the circuit board the you are trying to create to help the forum understand what the "real world" trigger is. That is, a final stage that swings a voltage from GND to 5V should be easy but what is the stimulus or logic that causes the need to trigger the WAV tr...
by exeng
Mon Feb 05, 2018 12:13 am
Forum: SparkFun Product Questions
Topic: WAV Trigger voltage signal
Replies: 10
Views: 436

Re: WAV Trigger voltage signal

I stand corrected. As I said I've not interfaced with the WAV Trigger in that configuration. Everything I do is though the serial interface.
by exeng
Sun Feb 04, 2018 3:10 pm
Forum: Arduino
Topic: Help With if/else Statement
Replies: 12
Views: 446

Re: Help With if/else Statement

Your welcome.
by exeng
Sun Feb 04, 2018 3:08 pm
Forum: SparkFun Product Questions
Topic: WAV Trigger voltage signal
Replies: 10
Views: 436

Re: WAV Trigger voltage signal

Watch the video here https://learn.sparkfun.com/tutorials/wav-trigger-hookup-guide-v11?_ga=2.22275833.358574595.1517520130-277886375.1504673727 and look that the schematic here https://cdn.sparkfun.com/datasheets/Widgets/wavtrigger_v11.pdf for clues on how to connect to the trigger inputs. I've not ...
by exeng
Sun Feb 04, 2018 10:36 am
Forum: Arduino
Topic: Help With if/else Statement
Replies: 12
Views: 446

Re: Help With if/else Statement

Well damn you paulvha (just kidding) you beat me to it. Must be a time zone time. Yes that will work. I had just this morning (PST) finished my version (very similar) and was about to post when I saw this. The difficult part was trying to understand what Ardalan wanted. Once he described it in full ...
by exeng
Sat Feb 03, 2018 11:37 pm
Forum: Arduino
Topic: Help With if/else Statement
Replies: 12
Views: 446

Re: Help With if/else Statement

OK, so what may be happening is that once you enter the <50 state you are toggling your state variable at a rate roughly equivalent to 500ms delay and driving your on/off LED accordingly. If you want to slow down the toggle than yes, adjust the delay. But to me that may not be the behavior you reall...
by exeng
Sat Feb 03, 2018 10:46 pm
Forum: Arduino
Topic: Help With if/else Statement
Replies: 12
Views: 446

Re: Help With if/else Statement

Perhaps this will help me understand your desired behavior... Assuming currentState is initialized to 0, what would be the expected values of currentState (abbv. CS in the table below) for each read of distance: Of course Last CS will = New CS of any prior read. [Read],Distance < 50],[Last CS],[New ...
by exeng
Sat Feb 03, 2018 9:55 pm
Forum: Arduino
Topic: Help With if/else Statement
Replies: 12
Views: 446

Re: Help With if/else Statement

Need some clarification... You say I want to toggle "currentState" between 0 and 1 for every 1 time distance becomes less than 50. Do you mean if it's less than 50 on any read, then toggle currentState. Or to you mean toggle currentState when less than 50 if and only if the prior read was not less t...
by exeng
Sat Feb 03, 2018 2:00 pm
Forum: Arduino
Topic: Testing if a 230v AC circuit is closed
Replies: 5
Views: 296

Re: Testing if a 230v AC circuit is closed

Does this unit have any display or power indicators driven by 5v logic? If so you could potentially tap into an LED's anode lead that comes on when power is on. I did this for a camera that I wanted to time lapse control with a micro controller. I needed to know if the camera was on or not when it w...