Search found 32 matches

by alim
Mon Mar 06, 2017 11:19 pm
Forum: Projects
Topic: Laser driver
Replies: 0
Views: 334

Laser driver

Hello everyone, I am working on a project that needs to have a laser driver. Actually a laser array, so total current is around 2A. I am using LD39300 for creating a voltage driver, since it can supply upto 3A current. What I am facing is the at full power, driver runs for 30-40 mins and then starts...
by alim
Fri Jan 20, 2017 10:18 pm
Forum: Wireless/RF
Topic: Bluetooth silvermate
Replies: 1
Views: 484

Re: Bluetooth silvermate

I did some extra test. Here is my results. If I follow this following link: http://arduinoandroid.blogspot.com/2011/11/post-number-2-work-version.html Using $$$ command does not do anything. If I try to send a signal via bluetooth, serial port read it as giberish. I am kind of lost here. Anyone has ...
by alim
Thu Jan 05, 2017 3:12 pm
Forum: Wireless/RF
Topic: Bluetooth silvermate
Replies: 1
Views: 484

Bluetooth silvermate

Hello, I bought bluetooth silver mate from sparkfun. I used the instructions from following link: https://learn.sparkfun.com/tutorials/using-the-bluesmirf?_ga=1.128157772.1585294772.1400889417 Everything works fine when I use pro mini 5V (16 MHz), however if I use pro min 3.3V (8MHz), nothing works....
by alim
Thu Dec 22, 2016 6:33 pm
Forum: SparkFun Product Questions
Topic: 3.3Voltage regulator with low dropout
Replies: 1
Views: 340

3.3Voltage regulator with low dropout

Hello, I have bought 3.3V regulator (https://www.sparkfun.com/products/526) from sparkfun. I am using a battery, it output is 3.7V; so output of voltage regulator becomes like 2.7V which is not good enough to run Arduino. In this case voltage dropout is 1V. I am just wondering if you know any soluti...
by alim
Sun Sep 18, 2016 10:13 am
Forum: Arduino
Topic: Time to excute command
Replies: 3
Views: 510

Re: Time to excute command

Wonderful, thank you both.
by alim
Sat Sep 17, 2016 4:18 pm
Forum: Arduino
Topic: Time to excute command
Replies: 3
Views: 510

Time to excute command

Hello everyone, In one of my project, I am using interrupt and my microcontroller is Arduino Pro mini (5V, 16MHz) ATMega328. I am using both interrupts. Under each interrupt I am calling a function like following: detachInterrupt(0); A_SIG=1; B_SIG=digitalRead(PinB); // PinB is another interrupt pin...
by alim
Sun Sep 11, 2016 6:41 pm
Forum: SparkFun Product Questions
Topic: Small LCD
Replies: 2
Views: 325

Re: Small LCD

Thanks Mike for your quick reply. I believe it will be easy for me to go with LCD-00258. Using LCD-00258 to Arduino is very simple (just one pin) and it's library is also available.
I am wondering if I can know the connection between LCD-11122 and LCD-00258. Any link will be good. Thanks in advance.
by alim
Sun Sep 11, 2016 12:15 pm
Forum: SparkFun Product Questions
Topic: Small LCD
Replies: 2
Views: 325

Small LCD

Hello all; I bought one small lcd (i.e. LCD-11122). It needs 11 input/output pins for microcontroller interfacing. I am using Arduino pro mini which has 14 I/O pins. So, if I use this LCD, then I do not have enough pins to add more peripherals. I like the size of this LCD and pro-min for my project....
by alim
Thu Jul 21, 2016 3:26 pm
Forum: Projects
Topic: Laser Power Meter
Replies: 0
Views: 410

Laser Power Meter

Hello everyone, I am looking for power meter. I will be using two different types of lasers, one is visible laser and another one is infrared laser. In my project, laser power will vary in different phase. So, I am looking for a meter to measure laser power. Please let me know if you have any knowle...
by alim
Wed Jul 20, 2016 4:41 pm
Forum: SparkFun Product Questions
Topic: small stepper motor
Replies: 9
Views: 786

Re: small stepper motor

Just want to mention that one have to use AC power source for this purpose. DC power source, one must use driver.
by alim
Wed Jul 20, 2016 3:59 pm
Forum: SparkFun Product Questions
Topic: small stepper motor
Replies: 9
Views: 786

Re: small stepper motor

@Valen and all, sorry if I made you upset about this question. I was looking for a quick solution where I have to use stepper motor but I do not need to count steps. I know dc motor is the best choice here. However, the required rpm is low for my application and do not want to use dc motor which can...
by alim
Tue Jul 19, 2016 4:01 pm
Forum: SparkFun Product Questions
Topic: small stepper motor
Replies: 9
Views: 786

Re: small stepper motor

I actually found the solution. Yes stepper motor can be run without a driver. You can find solution in youtube.
by alim
Mon Jul 18, 2016 7:59 pm
Forum: SparkFun Product Questions
Topic: small stepper motor
Replies: 9
Views: 786

small stepper motor

Hello everyone,
I have bought small stepper motor (https://www.sparkfun.com/products/10551) from sparkfun. I will run this motor in one direction only and in a constant speed. Is there any way, I can run this motor without driver? This will reduce my product costs and complexity.
by alim
Sat Jul 16, 2016 10:42 am
Forum: SparkFun Product Questions
Topic: Lilypad connections
Replies: 0
Views: 314

Lilypad connections

Hello, I am very new in wearable electronics. I have collected few components such as Lilypad main 328 board, Sparkfun Bluetooth Mate silter, temperature sensor, Lipo charge Basic, etc. I am facing problem to connect one to other. It seems I have to have alligator connector in one side (i.e. main bo...
by alim
Thu Jul 14, 2016 1:23 pm
Forum: Projects
Topic: Laser power controller
Replies: 6
Views: 749

Re: Laser power controller

Lyndon, I do not think I can choose 3-10A output. I had to select first "Packaging", then voltage output, voltage input, then package case, finally supply device package (either D-PAK or PPAK). I am using digi-key.com here. Am I missing anything?