SparkFun Forums 

Where electronics enthusiasts find answers.

Search found 19 matches

 Go to advanced search

Re: RFM69HCW and Arduino Uno R3 Problem

 by jack0987 ¦  Thu Sep 20, 2018 3:18 pm ¦  Forum: Wireless/RF ¦  Topic: RFM69HCW and Arduino Uno R3 Problem ¦  Replies: 6 ¦  Views: 443

jack0987 wrote: Tue Sep 18, 2018 11:59 am
jack0987 wrote: Mon Sep 10, 2018 7:31 am
... I noticed that the brown colored line (D2) in the tutorial has no translator.
Is this OK?
Did anyone pick up on this?
Should the brown line (wire) in the tutorial have a 5V to 3V converter?
Did anyone pick up on this?

Re: RFM69HCW and Arduino Uno R3 Problem

 by jack0987 ¦  Thu Sep 20, 2018 3:17 pm ¦  Forum: Wireless/RF ¦  Topic: RFM69HCW and Arduino Uno R3 Problem ¦  Replies: 6 ¦  Views: 443

I this exact set-up all the time and works perfectly so you must be doing something wrong or something is fried... Did you use signal translators ? The Uno is 5V and the RFM69 is 3V. Got it working now. A failed solder connection may have been the problem. I resoldered all of the connections and ch...

Re: RFM69HCW and Arduino Uno R3 Problem

 by jack0987 ¦  Tue Sep 18, 2018 11:59 am ¦  Forum: Wireless/RF ¦  Topic: RFM69HCW and Arduino Uno R3 Problem ¦  Replies: 6 ¦  Views: 443

jack0987 wrote: Mon Sep 10, 2018 7:31 am
... I noticed that the brown colored line (D2) in the tutorial has no translator.
Is this OK?
Did anyone pick up on this?
Should the brown line (wire) in the tutorial have a 5V to 3V converter?

Re: RFM69HCW and Arduino Uno R3 Problem

 by jack0987 ¦  Mon Sep 10, 2018 7:31 am ¦  Forum: Wireless/RF ¦  Topic: RFM69HCW and Arduino Uno R3 Problem ¦  Replies: 6 ¦  Views: 443

I this exact set-up all the time and works perfectly so you must be doing something wrong or something is fried... Did you use signal translators ? The Uno is 5V and the RFM69 is 3V. Thanks. At least you confirmed to me that this setup will work. I did use signal translators but I noticed that the ...

Re: Problem using RFM69HCW with a YUN (Generation 1) using SS on D9

 by jack0987 ¦  Mon Sep 10, 2018 6:13 am ¦  Forum: Wireless/RF ¦  Topic: Problem using RFM69HCW with a YUN (Generation 1) using SS on D9 ¦  Replies: 6 ¦  Views: 672

The SparkFun RFM69HCW Breakout and a Arduino Uno R3 combo is not working for me.
Please see topic
https://forum.sparkfun.com/viewtopic.php?f=13&t=48531

RFM69HCW and Arduino Uno R3 Problem

 by jack0987 ¦  Mon Sep 10, 2018 5:49 am ¦  Forum: Wireless/RF ¦  Topic: RFM69HCW and Arduino Uno R3 Problem ¦  Replies: 6 ¦  Views: 443

I am following this tutorial: RFM69HCW Hookup Guide https://learn.sparkfun.com/tutorials/rfm69hcw-hookup-guide For one node, I am using the RFM69HCW and a Arduino Uno R3. This combination is not working properly for me. I have it wired the same as for the 5V Redboard in the tutorial. I am using the ...

Wireless Mailbox Alert Project

 by jack0987 ¦  Thu Aug 09, 2018 11:20 am ¦  Forum: Wireless/RF ¦  Topic: Wireless Mailbox Alert Project ¦  Replies: 0 ¦  Views: 517

My mailbox is a distance away and many times I have gone up there only to find there is no mail or they have not come yet. There are many alert systems for sale on the market, but it is my understanding that for the most part their range is short or they work unreliably or both. Therefore, I would l...

Re: Size of Circuit Board Trace Width

 by jack0987 ¦  Thu Feb 19, 2015 12:48 am ¦  Forum: Projects ¦  Topic: Size of Circuit Board Trace Width ¦  Replies: 11 ¦  Views: 1032

Thank you Dave, rrpilot, and qwertymodo for your considered responses. Perhaps, at the present time, some of what you talk about is beyond my level of understanding. In any case, when I tried to use the calculator and came up with 1.28 mils it just did not seem right. I will use 5 volts. The amps wi...

Re: Size of Circuit Board Trace Width

 by jack0987 ¦  Tue Feb 17, 2015 6:44 am ¦  Forum: Projects ¦  Topic: Size of Circuit Board Trace Width ¦  Replies: 11 ¦  Views: 1032

Thanks for your reply. Using this calulator and entering 0.2 amp with a trace length of 5: http://www.circuitcalculator.com/wordpress/2006/01/31/pcb-trace-width-calculator/ I come up with 1.28 mils. Do you come up with the same thing? What if the voltage was 500 volts instead of the 5 volts I intend...

Re: Size of Circuit Board Trace Width

 by jack0987 ¦  Mon Feb 16, 2015 10:18 pm ¦  Forum: Projects ¦  Topic: Size of Circuit Board Trace Width ¦  Replies: 11 ¦  Views: 1032

Your answer, I believe, assumes I have not googled this. I have but am not sure I am doing it right and came here for confirmation and prehaps some helpful tips. For example, I see no entry on the calculator for voltage. In addition, the lmgtfy website appears to me to be what I call a spam site. I ...

Size of Circuit Board Trace Width

 by jack0987 ¦  Mon Feb 16, 2015 2:26 pm ¦  Forum: Projects ¦  Topic: Size of Circuit Board Trace Width ¦  Replies: 11 ¦  Views: 1032

What should the trace width on a 1oz. copper Board be for 5 volts, no more than 200ma, at normal operating temperatures?

Re: opto isolator causes indicators to dim

 by jack0987 ¦  Mon Sep 15, 2014 7:28 pm ¦  Forum: Arduino ¦  Topic: opto isolator causes indicators to dim ¦  Replies: 12 ¦  Views: 1673

I think I am getting somewhere using a transistor inverter with a 3904 which is what everyone was trying to explain to me above but I did not understand it and was not doing it right. R3 is there for a reason but may not be the correct value. In some cases the source led high/low voltage can vary an...

Re: opto isolator causes indicators to dim

 by jack0987 ¦  Mon Sep 15, 2014 2:29 pm ¦  Forum: Arduino ¦  Topic: opto isolator causes indicators to dim ¦  Replies: 12 ¦  Views: 1673

The source contains a current limiting resistor.

I am using a 3906 as I can not seem to get a 3904 to work.

Re: opto isolator causes indicators to dim

 by jack0987 ¦  Mon Sep 15, 2014 1:10 pm ¦  Forum: Arduino ¦  Topic: opto isolator causes indicators to dim ¦  Replies: 12 ¦  Views: 1673

This is sort of what I had in mind (but not quite) and it appears to be working. I had to lower the value of R4 because led2 was dimly lit when led1 was on. example1-small copy.jpg Note that the cathode of led2 is connected to Q1. I do not want it to be this way. I want the cathode to connect direct...

Re: opto isolator causes indicators to dim

 by jack0987 ¦  Mon Sep 15, 2014 11:31 am ¦  Forum: Arduino ¦  Topic: opto isolator causes indicators to dim ¦  Replies: 12 ¦  Views: 1673

I do not think I am doing it right. Is there a circuit diagram available on the web?