Search found 8 matches

by electronicsbasecom
Tue Feb 12, 2013 1:56 pm
Forum: SparkFun Product Questions
Topic: IOIO-OTG with Bluetooth Dongle Q
Replies: 3
Views: 992

Re: IOIO-OTG with Bluetooth Dongle Q

Did you pair dongle and Android Pad? Pairing code is 4545.
by electronicsbasecom
Fri Sep 14, 2012 1:30 pm
Forum: Wireless/RF
Topic: GE864-GPS - GPS_ON_OFF?
Replies: 1
Views: 664

Re: GE864-GPS - GPS_ON_OFF?

I am very happy to found this post. From same reason I start to make new design with GE864-GPS. You already helpped me, but I expect more. Now I see that pull-down on GPS_ON_OFF will not turn-on GPS. First...I saw youtube videos that sows how to reflow BGA...search it... Second...I will be very grat...
by electronicsbasecom
Thu Sep 06, 2012 4:21 pm
Forum: SparkFun Product Questions
Topic: 16VAC to 5VDC
Replies: 10
Views: 1854

Re: 16VAC to 5VDC

leon_heller wrote:It depends on the current.
LM2576 for 3A
or LM2575 for 1A
by electronicsbasecom
Wed Sep 05, 2012 3:04 pm
Forum: Wireless/RF
Topic: Telit - Listen Socket Problem
Replies: 1
Views: 712

Re: Telit - Listen Socket Problem

I can't see the pictures or download them....
by electronicsbasecom
Thu Jul 26, 2012 8:38 am
Forum: SparkFun Site Questions/Comments
Topic: FT232RL Solder Jumper Picture
Replies: 12
Views: 49609

Re: FT232RL Solder Jumper Picture

Hello, Since many comercial sollution with FT232 chip has no support for 3v3 level, I make my own board that is configurable by jumpers. Also, embeded MAX232 chip and DB9 port is usefull for other devices with MAX232 (for example GPRS modems, eV. kits etc. More informations you can find on following...
by electronicsbasecom
Sun Mar 25, 2012 7:53 am
Forum: PIC Microcontrollers - Software and Hardware
Topic: mTouch with PIC12F/LF1822
Replies: 1
Views: 1513

Re: mTouch with PIC12F/LF1822

i believe it will be much easier to adjust 16f707 code since 16 families are much more similar. are you using CSM or CTMU capacitive sensing? maybe it will ok for you to choose microcontroller with CSM module since i tested it and it gave great results. i wrote about it here http://forum.sparkfun.co...
by electronicsbasecom
Sat Mar 24, 2012 2:05 pm
Forum: SparkFun Product Questions
Topic: Using a battery as a touch sensor
Replies: 11
Views: 3530

Re: Using a battery as a touch sensor

May i advise you to use microcontrollers with integrated capacitance touch sensing module. I used Microchip mTouch and it is working flawless. i was able to detect finger press through 10mm glass easy.. :) if you want to work with it i made few tutorials as well as one complete project with source c...
by electronicsbasecom
Sat Mar 24, 2012 1:59 pm
Forum: PIC Microcontrollers - Software and Hardware
Topic: ~fF Capacitance measurement with mTouch 16f707 touch button!
Replies: 0
Views: 1255

~fF Capacitance measurement with mTouch 16f707 touch button!

Recently I started to work with mTouch CSM module. It sounded like extremely interesting and high performance hardware to work with. It sounded right! :) there are countless applications for use of this hardware. Touch pad, proximity sensors, readout of capacitive sensors,extreme precision capacitan...