SparkFun Forums 

Where electronics enthusiasts find answers.

Search found 8 matches

 Go to advanced search

Re: nRF24AP1 - ANT Code - Garmin Heart-Rate Monitor

 by deswong ¦  Sun Jan 22, 2012 7:29 pm ¦  Forum: Wireless/RF ¦  Topic: nRF24AP1 - ANT Code - Garmin Heart-Rate Monitor ¦  Replies: 72 ¦  Views: 40585

It is possible to use AntWare II to interface temporarily to the nRF24AP1 to determine if it is faulty?

Re: nRF24AP1 - ANT Code - Garmin Heart-Rate Monitor

 by deswong ¦  Sun Jan 22, 2012 6:50 pm ¦  Forum: Wireless/RF ¦  Topic: nRF24AP1 - ANT Code - Garmin Heart-Rate Monitor ¦  Replies: 72 ¦  Views: 40585

Could it be a fault with a batch of them perhaps? I have not had any luck in the last two months of owning one of these boards, is there any other troubleshooting that anyone else can suggest before putting the board down as faulty? I saw in another post that a user had the same issues, and a new bo...

Re: Troubleshooting nRF24AP1 with Trace Antenna

 by deswong ¦  Wed Jan 11, 2012 8:12 pm ¦  Forum: Wireless/RF ¦  Topic: Troubleshooting nRF24AP1 with Trace Antenna ¦  Replies: 5 ¦  Views: 808

How are you connecting to the nRF24AP1? What are you using to send messages to it? Also make sure that you are using the proper voltage levels (3.3v) and baud rate (4800bps).

Re: Nordic USB ANT Stick - Change the Baud Rate

 by deswong ¦  Tue Dec 13, 2011 8:01 pm ¦  Forum: Wireless/RF ¦  Topic: Nordic USB ANT Stick - Change the Baud Rate ¦  Replies: 1 ¦  Views: 540

There should be a BR1 and a BR2 on the rear of the board - these can be soldered across which then will change the baud rate for the receiver. I don't know which ones need to be bridged for what, except leaving them unbridged gets you the 4800baud async. The options are 4800baud, 19.2Kbaud, 38.4Kbau...

Re: nRF24AP1 - ANT Code - Garmin Heart-Rate Monitor

 by deswong ¦  Sun Dec 11, 2011 11:39 pm ¦  Forum: Wireless/RF ¦  Topic: nRF24AP1 - ANT Code - Garmin Heart-Rate Monitor ¦  Replies: 72 ¦  Views: 40585

Hi, I'm trying also to get this code working with Suunto HRM, but my code doesn't go past " int ANT_rxHandler() { Serial.println("ANT_rxHandler"); //Debugging int n, fd, rc, inmsg = FALSE; UCHAR chr, msgN; while (mySerial.available()>0) { " Meaning it doesn't do anything inside the While loop. So i...

Re: nRF24AP1 - ANT Code - Garmin Heart-Rate Monitor

 by deswong ¦  Mon Nov 28, 2011 8:33 pm ¦  Forum: Wireless/RF ¦  Topic: nRF24AP1 - ANT Code - Garmin Heart-Rate Monitor ¦  Replies: 72 ¦  Views: 40585

This is the wiring diagram that I have quickly put together (I could have drawn this by hand faster but I am at work) which is how I currently have my device connected to my pc.

diagram1.PNG

Re: nRF24AP1 - ANT Code - Garmin Heart-Rate Monitor

 by deswong ¦  Mon Nov 28, 2011 6:57 pm ¦  Forum: Wireless/RF ¦  Topic: nRF24AP1 - ANT Code - Garmin Heart-Rate Monitor ¦  Replies: 72 ¦  Views: 40585

Has anyone been able to successfully pair with this device: GARMIN 010-10997-00 Heart Rate Monitor http://new.digifit.com/hrm-garmin-heart-rate-monitor/index.asp I have been having difficulty in getting this working with the nRF24AP1 - I have tested this on another ANT compatible machine (Concept2 R...

Re: nRF24AP1 - ANT Code - Garmin Heart-Rate Monitor

 by deswong ¦  Sun Nov 27, 2011 10:01 pm ¦  Forum: Wireless/RF ¦  Topic: nRF24AP1 - ANT Code - Garmin Heart-Rate Monitor ¦  Replies: 72 ¦  Views: 40585

I'm getting this error...I've linked to the NewSoftSerial library. I'm an old fart trying to learn something new...any help is greatly appreciated.... sketch_nov15b.cpp: In function 'int ANT_rxHandler()': sketch_nov15b:528: error: 'class SoftwareSerial' has no member named 'available' Hi Connorly, ...