Search found 6 matches

by sswcharlie
Wed Oct 24, 2018 11:43 pm
Forum: Arduino
Topic: Arduino Variable speed dc motor with BLE
Replies: 0
Views: 44

Arduino Variable speed dc motor with BLE

Hi Can someone refer me to a sketch that uses Uno and BLE and motorshield that receives a message via ble from smart phone, and adjusts the 12 volt dc motor speed (28 steps!) from zero to full speed. The motor will receive power from a 12 volt battery. Smartphone app etc ok. An Ardublock would be gr...
by sswcharlie
Wed Jan 17, 2018 11:48 pm
Forum: Arduino
Topic: ArduBlock in Reverse
Replies: 0
Views: 301

ArduBlock in Reverse

Is it possible to load working Arduino sketch onto ArduBlock and get a ArduBlock example ? So user can underestand the setup and loop codes etc
Thks
Charles Harris
by sswcharlie
Wed Jan 17, 2018 11:42 pm
Forum: Arduino
Topic: Arduino Block type Programming - Which one
Replies: 1
Views: 272

Re: Arduino Block type Programming - Which one

Can anyone help with my question?
Thanks
by sswcharlie
Mon Dec 18, 2017 5:49 pm
Forum: Arduino
Topic: Arduino Block type Programming - Which one
Replies: 1
Views: 272

Arduino Block type Programming - Which one

Hi Noobie. Looking at purchasing a Uno with BLE and a motor shield. For a beginner what is the best/easiest block type program to use. All I want to do is to have a BT device with a variable speed slider and 2 button (fwd and rev), So blocks will include BLE connection and motor control via shield. ...
by sswcharlie
Mon May 27, 2013 6:47 pm
Forum: SparkFun Product Questions
Topic: SPE AVR Stick
Replies: 0
Views: 263

SPE AVR Stick

Hi Trying to sort what this stick can do. I want to feed into the stick by usb serial numbers only from multiple rfid reader, time stamp and add a prefix and on into MS Excel. The problem I have is with the rfid readers they are all the same and all have same product id etc. However they do show up ...
by sswcharlie
Fri Sep 02, 2011 11:35 pm
Forum: SparkFun Product Questions
Topic: Wearable Keypad
Replies: 0
Views: 193

Wearable Keypad

Hi

Could this device be fitted to a usb connection to laptop ? What would need to be done ? For use in getting around a spreadsheet.

Thanks

Charlie