SparkFun Forums 

Where electronics enthusiasts find answers.

Search found 5 matches

 Go to advanced search

 by adr1an ¦  Tue Aug 18, 2009 6:07 pm ¦  Forum: New Product Ideas ¦  Topic: Mini-PVR (Low-Res vid capture to SD) ¦  Replies: 5 ¦  Views: 1628

That's about where my FPGA experience finishes. Someone else is going to need to chime in, but I can tell you it won't be a straightforward process. It is a whole project in itself. Then again, it depends what your image sensor is. If it is one of those UART/Serial JPEG cameras then it is quite sim...

 by adr1an ¦  Tue Aug 18, 2009 9:35 am ¦  Forum: New Product Ideas ¦  Topic: Mini-PVR (Low-Res vid capture to SD) ¦  Replies: 5 ¦  Views: 1628

You would most likley need some sort of FPGA for that, add in compression and it becomes a bit more complex... There are no single chip solutions that do what you want (apart from the kind of ASIC's in video cameras etc). I'm being harrased to look at incorporating this somehow into my current proj...

Mini-PVR (Low-Res vid capture to SD)

 by adr1an ¦  Tue Aug 18, 2009 7:25 am ¦  Forum: New Product Ideas ¦  Topic: Mini-PVR (Low-Res vid capture to SD) ¦  Replies: 5 ¦  Views: 1628

It would be awesome if there was some BoB that allowed low-res (320line or there abouts PAL) video capture to SD. Something that either captured to an on-BoB microSD slot or used SPI to talk to an external one. Even if it used a custom filesystem, or did raw, as long as you could read it back on a P...

 by adr1an ¦  Thu Jul 30, 2009 10:36 pm ¦  Forum: Code ¦  Topic: Mega + MAX7456 Breakout ¦  Replies: 5 ¦  Views: 3499

*bump*

I've tried with a 10k resistor tied between reset and V+ as a suggestion from the arduino.cc forums, but still no luck.

Mega + MAX7456 Breakout

 by adr1an ¦  Sun Jul 26, 2009 10:22 pm ¦  Forum: Code ¦  Topic: Mega + MAX7456 Breakout ¦  Replies: 5 ¦  Views: 3499

Hi all. I'm horribly stuck with this breakout and wonder if anyone can offer some insight. I have it hooked up to ports 50-53 and INT0 (D2) and am using the code supplied in the thread http://www.arduino.cc/cgi-bin/yabb2/YaBB.pl?num=1220054359/59#59 over at arduino.cc. As you can see described in th...