SparkFun Forums 

Where electronics enthusiasts find answers.

Search found 2882 matches

 Go to advanced search

Re: Detecting XBee Packet Transmission

 by stevech ¦  Mon Jun 13, 2016 9:55 pm ¦  Forum: Wireless/RF ¦  Topic: Detecting XBee Packet Transmission ¦  Replies: 1 ¦  Views: 1112

receiving XBee will alter its received signal strength indicator (RSSI) as each packet is received. That pin on the XBee can be observed.

Re: wireless anti theft device

 by stevech ¦  Fri Jun 10, 2016 9:37 am ¦  Forum: Wireless/RF ¦  Topic: wireless anti theft device ¦  Replies: 2 ¦  Views: 1109

yes. Most all laptops/tablets have a slot compatible with
http://www.kensington.com/us/us/4http:/ ... 1rsFaJrWYg

Re: Rotary encoder - misses steps

 by stevech ¦  Sun May 29, 2016 10:40 pm ¦  Forum: Projects ¦  Topic: Rotary encoder - misses steps ¦  Replies: 11 ¦  Views: 1417

@stevech: If you only allow valid transitions of the encoder edges through the various quadrature states, do you find that the SF encoder still needs debouncing? I've used that technique with noisy mechanical encoders and found that it gives me error free operation. Although I will admit that I hav...

Re: XBee Series 1... what else to buy?

 by stevech ¦  Fri May 27, 2016 10:10 pm ¦  Forum: Wireless/RF ¦  Topic: XBee Series 1... what else to buy? ¦  Replies: 3 ¦  Views: 908

WHy not get Arduino boards that are 3.3V?

Re: data communication using radio

 by stevech ¦  Fri May 27, 2016 12:30 am ¦  Forum: Projects ¦  Topic: data communication using radio ¦  Replies: 9 ¦  Views: 1862

The RS232 standard permits voltages compatible with what you are seeing with the max232.

Check data polarity inversions from end to end. Probably one inversion in the Max232.

Re: Rotary encoder - misses steps

 by stevech ¦  Mon May 23, 2016 7:14 pm ¦  Forum: Projects ¦  Topic: Rotary encoder - misses steps ¦  Replies: 11 ¦  Views: 1417

I just went through getting the SFE rotary encoder to work properly. If I can summarize... Must get interrupt from both A and B phase and on both rising and falling edge - in order to fully debounce the switches. Sometimes they glitch while gliding along the conductive strip. Debouncing slow rotatio...

Re: Arduino XBee S1 API frame read problem

 by stevech ¦  Thu May 19, 2016 10:36 pm ¦  Forum: Wireless/RF ¦  Topic: Arduino XBee S1 API frame read problem ¦  Replies: 2 ¦  Views: 1391

Use an Ardino or Raspberry Pi/Python XBee library. All work is done for you.

API mode frames vary in length and format. It is a lot to learn to do API coding rather than using a library.

Re: automatic garage door closer

 by stevech ¦  Thu May 19, 2016 10:25 pm ¦  Forum: Projects ¦  Topic: automatic garage door closer ¦  Replies: 3 ¦  Views: 726

yes, here's my experiences... I bought one of these automatic door closers on sale... http://www.skylinkhome.com/usa/universal_garage_one.html There are others. It has a battery powered on-door sensor for door-is-closed. A plunger-switch that hits the ground. Wireless message to control unit. Contro...

Re: Alternative connector to RJ45 Jack for Ethernet

 by stevech ¦  Mon May 16, 2016 5:36 pm ¦  Forum: Projects ¦  Topic: Alternative connector to RJ45 Jack for Ethernet ¦  Replies: 4 ¦  Views: 1039

yes.. the transformer is inside some RJ-45's

Re: Alternative connector to RJ45 Jack for Ethernet

 by stevech ¦  Sat May 14, 2016 3:51 pm ¦  Forum: Projects ¦  Topic: Alternative connector to RJ45 Jack for Ethernet ¦  Replies: 4 ¦  Views: 1039

RJ-11 phone jack. but connector for cable would be special too.

for short runs, phone cables can be used.. cat-3.

Re: Geofencing

 by stevech ¦  Sun May 01, 2016 9:25 pm ¦  Forum: Wireless/RF ¦  Topic: Geofencing ¦  Replies: 2 ¦  Views: 959

Im wondering if i can reduce the range of a bluetooth device or how it would be possible for me to make some kind of device that could only go a certain amount of meters from the source. And if i could set it on the go with an app or something. Yes, geofencing is restricting movements to inside a p...

Re: Unable to run Atmega32u4 at 3.3v

 by stevech ¦  Sat Apr 30, 2016 10:38 pm ¦  Forum: AVR Microcontrollers ¦  Topic: Unable to run Atmega32u4 at 3.3v ¦  Replies: 2 ¦  Views: 1753

I am using an atmega32u4 microcontroller in my project. The 32u4 is connected in my project in a same way as that of atmega32u4 breakout board from sparkfun. In my project the 32U4 is connected to 5v and 16mhz crystal oscillator and it works fine and gets detected by my PC. But my project requires ...

Re: Xbee ZigBee Pro (S2C) with Anaren AIR ZigBee

 by stevech ¦  Tue Apr 26, 2016 10:21 pm ¦  Forum: Wireless/RF ¦  Topic: Xbee ZigBee Pro (S2C) with Anaren AIR ZigBee ¦  Replies: 1 ¦  Views: 930

I worked with these TI parts for quite some time, professionally. I gave up. So did Anaren, apparently.
T.I. is sending too much to Bangalore.

Re: Can someone give me a basic overview of Arduino, please?

 by stevech ¦  Tue Apr 26, 2016 10:14 pm ¦  Forum: Arduino ¦  Topic: Can someone give me a basic overview of Arduino, please? ¦  Replies: 18 ¦  Views: 1787

lyndon wrote:I'm well aware of the problem of counterfeit parts, but at these prices, I'll take the risk.
So it's OK to steal intellectual property, use another company's logo and fake part numbers, and so on?

That's just nice.

Re: Can someone give me a basic overview of Arduino, please?

 by stevech ¦  Thu Apr 14, 2016 12:09 am ¦  Forum: Arduino ¦  Topic: Can someone give me a basic overview of Arduino, please? ¦  Replies: 18 ¦  Views: 1787

lyndon wrote:
hcb wrote: I can buy the ATMega328P chips for about 3-4 dollars easily.
I can buy entire Arduinos for less than that!

Well, China will be happy to sell you a very fine thing indeed. Counterfeits and all.

  • 1
  • 2
  • 3
  • 4
  • 5
  • 193