Search found 17 matches

by static
Fri May 18, 2012 4:29 pm
Forum: SparkFun Site Questions/Comments
Topic: Simple parts inventory program? (free or opensource)
Replies: 21
Views: 35940

Re: Simple parts inventory program? (free or opensource)

Hi guys I've just deployed a web app that i created to help me keep track of my inventory. I figured why not share it with others. So i've added the login function (so everyone who signed up has their own inventory, duh ;) check it out: http://inventory.railified.com/ note: after you signup, click o...
by static
Mon Feb 09, 2009 9:32 am
Forum: PCB Design Questions
Topic: question about copper fill around holes
Replies: 3
Views: 964

sorry if i was unclear for example, you have a footprint of a part that contains holes (like an SD card connector for instance). But once i create a ground plane, it pours way too far from the actual holes, much further than the clearance set in the ground plan properties. I cannot seem to find a wa...
by static
Sun Feb 08, 2009 9:20 am
Forum: PCB Design Questions
Topic: question about copper fill around holes
Replies: 3
Views: 964

question about copper fill around holes

Hi

I'd like to change the copper fill clearance radius around regular drill holes. By default it is too large in eagle and breaks my ground planes too much.

how do i go about changing this radius, i've clicked around ground plane options but couldn't find

Thanks
Alex
by static
Thu Jan 22, 2009 4:16 pm
Forum: SparkFun Product Questions
Topic: 32 bit flash MCU deathmatch
Replies: 4
Views: 1464

Not sure why stm32 are not as popular here i tried atmel's ARM7 (sam7) and IMO STM32 is much more convenient and faster to boot. In general i like Cortexm3 much better than the old arm7 the other micro i use is Parallax Propeller and it's awesome, but for different kinds of projects than STM32 (i.e ...
by static
Sun Jan 11, 2009 5:01 pm
Forum: PCB Design Questions
Topic: Deutsch connectors!!!
Replies: 2
Views: 892

cheapest place i could find for this particular type, ask them, maybe they have other types of deutsch too

http://www.mefi-4.com/sc/details.asp?item=6pindeutsch
by static
Mon Dec 01, 2008 7:08 pm
Forum: PCB Design Questions
Topic: two quick questions on Eagle
Replies: 4
Views: 1441

two quick questions on Eagle

Hi 1. How can i copy a part from schematic in one file to another different schematic file? Same for .brd files - i.e a part of board layout - is it possible in eagle? 2. I see one can export a list of all parts used in schematic, but is it possible to have something like: resistor 1k x5 resistor 5k...
by static
Fri Nov 21, 2008 7:34 am
Forum: SparkFun Product Questions
Topic: Picking a Speaker
Replies: 11
Views: 1707

Unfortunately I don't think you will be very successful in implementing this. Besides looking at SPL you have to realize one important thing - to achieve the same SPL in lower frequencies, you'll need MORE energy than you would have needed to achieve same SPL in higher frequency. This is one Two: in...
by static
Sat Nov 01, 2008 8:58 pm
Forum: PCB Design Questions
Topic: Building a home made board with TQFP package
Replies: 23
Views: 15849

crocu wrote:Thank you very much silic0re for this link.

It is exactly what i'm looking for .
However, board cost about 9$ and shipping cost ~ 75 $ for France !
Is there a cheaper place to order ?
yes
http://futurlec.com/SMD_Adapters.shtml
by static
Sat Nov 01, 2008 8:36 pm
Forum: Everything ARM and LPC
Topic: Cortex-M3 (STM32) opensource development support
Replies: 7
Views: 3078

yes, latest codesourcery binaries (you don't have to build everything) work good for stm32 under cygwin as well as under ubuntu.

examples of environment/makefiles/project can be found by looking for name 'lanchon' (who has kindly shared his gcc based examples with community)
by static
Tue Oct 14, 2008 10:39 am
Forum: SparkFun Product Questions
Topic: anyone has problems with LIS3LV02 data output? continuity
Replies: 0
Views: 1114

anyone has problems with LIS3LV02 data output? continuity

Hi I've been working on a prototype, where a MCU gathers the accel data from the LIS3LV02DL (i use the DL version, not DQ) and sends x,y and z (both high and low bytes) as a simple bytestream over a serial port. The host PC collects the data and uses it to control a visual representation (modifies t...
by static
Tue Oct 14, 2008 10:13 am
Forum: SparkFun Product Questions
Topic: Missing bits when reading LIS3LV02DQ
Replies: 1
Views: 708

see the "Update" part here: http://www.nearfuturelaboratory.com/2006/09/22/arduino-and-the-lis3lv02dq-triple-axis-accelerometer/ it may be related to problem you're having edit: here is another thread dealing with seemingly the same issue: (or symptom anyway) http://forum.sparkfun.com/viewtopic.php?...
by static
Tue Oct 14, 2008 9:02 am
Forum: SparkFun Product Questions
Topic: Soldering QFN?
Replies: 26
Views: 8944

for prototyping, i found it very handy to fabricate a small DIP module as followings: - get a small piece of proto pcb (with grid of holes) that can contain the QFN package and the header connectors comfortably (i used x2 8pin single headers for the accelerator chip i did) - glue the QFN chip upside...
by static
Sat Oct 11, 2008 3:31 pm
Forum: OpenOCD
Topic: Config file for STM32 + Wiggler (new OpenOCD config format)
Replies: 4
Views: 3996

it appears i've been chasing my tail

forgot to include lib/src/stm32f10x_vector.o into the makefile

Cheers
by static
Fri Oct 10, 2008 5:41 pm
Forum: OpenOCD
Topic: Config file for STM32 + Wiggler (new OpenOCD config format)
Replies: 4
Views: 3996

ok, i think i found my problem i tried main.bin that i've compiled under windows (using codesourcery toolchain for windows under cygwin) and it works (and doesn't report "empty section 0") I am thinking something is wrong with the .ld files, or somehow the linux version of codesourcery doesn't creat...