- Fri Apr 13, 2007 2:08 pm
#28552
Anyone have an example of the nRF24L01 connected to a power amplifier? I have been looking at the MAX2240 by Maxim. The MAX2240 is a 100mw or +20dB power amplifier for 2.4 GHz ISM GFSK modulated radios.
Can I connect the MAX2240 directly to the ANT1 or ANT2 outputs of the nRF24L01 without the impedence network? I think the impedence network is still required to match the 50 ohm impedence but I want to make sure. The MAX2240 datasheet says it can accept a 50 ohm transmission line but it doesn't say it has to be 50 ohms. I am not too familiar with impedence matching on RF.
Also, the MAX2240 datasheet makes it seem like it is unidirectional from RF input to RF output. Is this true? Meaning, if I use the MAX2240, I can only transmit and not receive?
Any info would be appreciated. If this little chip turns out to work well and is easy to use, I would love to see a 100mw MiRF v2 with RP-SMA.
Thanks!
Nullz
Can I connect the MAX2240 directly to the ANT1 or ANT2 outputs of the nRF24L01 without the impedence network? I think the impedence network is still required to match the 50 ohm impedence but I want to make sure. The MAX2240 datasheet says it can accept a 50 ohm transmission line but it doesn't say it has to be 50 ohms. I am not too familiar with impedence matching on RF.
Also, the MAX2240 datasheet makes it seem like it is unidirectional from RF input to RF output. Is this true? Meaning, if I use the MAX2240, I can only transmit and not receive?
Any info would be appreciated. If this little chip turns out to work well and is easy to use, I would love to see a 100mw MiRF v2 with RP-SMA.
Thanks!
Nullz