- Tue Nov 30, 2010 12:25 pm
#114552
Couple of questions:
I've recently purchased two of the latest versions of this LED backpack (RGBSerialMatrixBackPack_UG_090420), and I'm having problems with daisy chaining from an Arduino Uno..
1. Both boards display the following colors upon booting in the lower left hand corner of the backpack: RRGGBB. From reading around on the net I understand that the second backpack in the daisy chain should identify itself as second in the chain by displaying a different pattern of colors in the lower left hand corner when booting. Is this correct? If so do I need to upgrade to a new version of the board firmware and if so where can I find that firmware?
2. Does anyone have a simple Arduino Sketch that utilizes a daisy chained series of these backpacks?
Many thanks!
I've recently purchased two of the latest versions of this LED backpack (RGBSerialMatrixBackPack_UG_090420), and I'm having problems with daisy chaining from an Arduino Uno..
1. Both boards display the following colors upon booting in the lower left hand corner of the backpack: RRGGBB. From reading around on the net I understand that the second backpack in the daisy chain should identify itself as second in the chain by displaying a different pattern of colors in the lower left hand corner when booting. Is this correct? If so do I need to upgrade to a new version of the board firmware and if so where can I find that firmware?
2. Does anyone have a simple Arduino Sketch that utilizes a daisy chained series of these backpacks?
Many thanks!