- Wed Feb 17, 2010 9:55 am
#93717
Hi,
Does anyone know if the Amtera USB blaster is supported by openOCD? It is mentioned (along with the config commands) on this page:
http://openocd.berlios.de/doc/html/Inte ... ation.html
Such as:
Tried with two versions. 0.3.1, and 2007re141. I have only ever successfully used the latter version, it is the same one used in Jim Lynch's wonderful tutorial.
I realise there is a patch for a 'USB blaster clone' on this page:
http://www.ixo.de/info/usb_jtag/
But I do'nt know how to use it with either version of OpenOCD. I would love to get this working, as I'm still having 'issues' with my FT2232 programer (JTAGkey based clone) - which could be hardware, or software,I don't know.
Hope someone can shed some light on this,
Blueteeth
Does anyone know if the Amtera USB blaster is supported by openOCD? It is mentioned (along with the config commands) on this page:
http://openocd.berlios.de/doc/html/Inte ... ation.html
Such as:
— Interface Driver: usb_blasterI have tried the bove commands but it is not recognised as an interface.
USB JTAG/USB-Blaster compatibles over one of the userspace libraries for FTDI chips. These interfaces have several commands, used to configure the driver before initializing the JTAG scan chain:
— Config Command: usb_blaster_device_desc description
Provides the USB device description (the iProduct string) of the FTDI FT245 device. If not specified, the FTDI default value is used. This setting is only valid if compiled with FTD2XX support.
— Config Command: usb_blaster_vid_pid vid pid
The vendor ID and product ID of the FTDI FT245 device. If not specified, default values are used. Currently, only one vid, pid pair may be given, e.g. for Altera USB-Blaster (default):
ft2232_vid_pid 0x09FB 0x6001
The following VID/PID is for Kolja Waschk's USB JTAG:
ft2232_vid_pid 0x16C0 0x06AD
Tried with two versions. 0.3.1, and 2007re141. I have only ever successfully used the latter version, it is the same one used in Jim Lynch's wonderful tutorial.
I realise there is a patch for a 'USB blaster clone' on this page:
http://www.ixo.de/info/usb_jtag/
But I do'nt know how to use it with either version of OpenOCD. I would love to get this working, as I'm still having 'issues' with my FT2232 programer (JTAGkey based clone) - which could be hardware, or software,I don't know.
Hope someone can shed some light on this,
Blueteeth