- Wed Mar 09, 2011 5:58 am
#122324
I am very new to arduino.
I got everything that needed mocked up and planned out on a Arduino Uno, one of the major things was the LS20031 GPS.
I used NSS to print out what i needed to Serial using the following code:
So i get just what i need with the Arduino Uno, but i would like a smaller package, so i got the arduino Mini Pro 3.3v 328.
I hook everything up the exact same as i did with the Uno and upload the same code. GPS powers on, gets a fix (red blinking light) but I am getting no Serial output.
I am stumped...anyone? Is there something about the Mini Pro that I am missing?
Thanks in advance!
I got everything that needed mocked up and planned out on a Arduino Uno, one of the major things was the LS20031 GPS.
I used NSS to print out what i needed to Serial using the following code:
Code: Select all
I also changed the line in NewSoftSerial.h _NewSS_MAX_RX_BUFF to 128.#include <NewSoftSerial.h>
#include <TinyGPS.h>
TinyGPS gps;
NewSoftSerial nss(2, 3);
int year, month, day, hour, minutes, second, hundredths;
unsigned long fix_age;
void gpsdump(TinyGPS &gps);
bool feedgps();
void printFloat(double f, int digits = 2);
void setup()
{
Serial.begin(115200);
nss.begin(57600);
}
void loop(){
bool newdata = false;
unsigned long start = millis();
// Every 5 seconds we print an update
while (millis() - start < 1000){
if (feedgps())
newdata = true;
}
if (newdata){
Serial.println("-------------");
gpsdump(gps);
Serial.println("-------------");
}
}
void printFloat(double number, int digits){
// Handle negative numbers
if (number < 0.0){
Serial.print('-');
number = -number;
}
// Round correctly so that print(1.999, 2) prints as "2.00"
double rounding = 0.5;
for (uint8_t i=0; i<digits; ++i)
rounding /= 10.0;
number += rounding;
// Extract the integer part of the number and print it
unsigned long int_part = (unsigned long)number;
double remainder = number - (double)int_part;
Serial.print(int_part);
// Print the decimal point, but only if there are digits beyond
if (digits > 0)
Serial.print(".");
// Extract digits from the remainder one at a time
while (digits-- > 0){
remainder *= 10.0;
int toPrint = int(remainder);
Serial.print(toPrint);
remainder -= toPrint;
}
}
void gpsdump(TinyGPS &gps){
long lat, lon;
float flat, flon;
unsigned long age, date, time, chars;
int year;
byte month, day, hour, minute, second, hundredths;
unsigned short sentences, failed;
feedgps(); // If we don't feed the gps during this long routine, we may drop characters and get checksum errors
gps.f_get_position(&flat, &flon, &age);
Serial.print("Lat/Long(float): "); printFloat(flat, 5); Serial.print(", "); printFloat(flon, 5);
feedgps();
gps.crack_datetime(&year, &month, &day, &hour, &minute, &second, &hundredths, &age);
if(month&&day&&year){
Serial.print("Date: "); Serial.print(static_cast<int>(month)); Serial.print("/");
Serial.print(static_cast<int>(day)); Serial.print("/");
Serial.print(year);
}
Serial.print(" Time: "); Serial.print(static_cast<int>(hour)); Serial.print(":");
Serial.print(static_cast<int>(minute)); Serial.print(":");
Serial.println(static_cast<int>(second));
}
bool feedgps(){
while (nss.available()){
if (gps.encode(nss.read()))
return true;
}
return false;
}
So i get just what i need with the Arduino Uno, but i would like a smaller package, so i got the arduino Mini Pro 3.3v 328.
I hook everything up the exact same as i did with the Uno and upload the same code. GPS powers on, gets a fix (red blinking light) but I am getting no Serial output.
I am stumped...anyone? Is there something about the Mini Pro that I am missing?
Thanks in advance!