Code: Select all/*
9-27-09
Copyright Spark Fun Electronics© 2009
Nathan Seidle
spark at sparkfun.com
Example Interface to AR1000
Using ATmega168 at 8MHz
Modified for Arduino:
6/29/2010
Robert Bennett
zeropointo at sparkfun.com
*/
#include <stdio.h>
#include <avr/io.h>
#include "i2c.h"
#define FOSC 8000000
#define BAUD 9600
#define MYUBRR 103
#define sbi(port, bit_mask) ((port) |= (uint8_t)(1 << bit_mask))
#define cbi(port, bit_mask) ((port) &= (uint8_t)~(1 << bit_mask))
#define STATUS_LED 5
#define AR1000_W 0x20 //Write address of AR1000
#define AR1000_R 0x21//read address
#define ADDR_STATUS 0x13 // the address of arStatus register
#define MASK_STC (1<<5) //0x0020 // Seek/Tune/PowerOn complete D5 in adress 13H
#define MASK_SF (1<<4) //0x0010 // Seek Fail D4 in address 13H
#define MASK_ST (1<<3) //0x0008 // Stereo D3 in address 13H
#define MASK_READCHAN 0xFF80 // D7~D15 in address 13H
#define SHIFT_READCHAN 7
#define AR1000_MUTE_ON { uint16_t temp = ar1000_read(1); ar1000_write(1, temp | (1<<1)); } //Reg_Data[1].BIT.B1 = ON;
#define AR1000_MUTE_OFF { uint16_t temp = ar1000_read(1); ar1000_write(1, temp & ~(1<<1)); } //Reg_Data[1].BIT.B1 = OFF;}
#define AR1000_TUNE_ON { uint16_t temp = ar1000_read(2); ar1000_write(2, temp | (1<<9)); } // Reg_Data[2].BIT.B9 = ON;
#define AR1000_TUNE_OFF { uint16_t temp = ar1000_read(2); ar1000_write(2, temp & ~(1<<9)); } //Reg_Data[2].BIT.B9 = OFF;
#define AR1000_SEEK_ON { uint16_t temp = ar1000_read(3); ar1000_write(3, temp | (1<<14)); } //Reg_Data[3].BIT.B14 = ON;}
#define AR1000_SEEK_OFF { uint16_t temp = ar1000_read(3); ar1000_write(3, temp & ~(1<<14)); } //Reg_Data[3].BIT.B14 = OFF;}
//I2CDEBUG will turn on '!' serial characters and TWI arStatus debugging
//Comment out the define to turn off debug characters
//#define I2CDEBUG
//Define functions
//======================
void i2c_SendStart(void);
void i2c_SendStop(void);
void i2c_WaitForComplete(void);
unsigned char i2c_SendByte(unsigned char data);
unsigned char i2c_ReceiveByte(unsigned char ackFlag);
void ioinit(void);
static int uart_putchar(char c, FILE *stream);
uint8_t uart_getchar(void);
int uart_gethex(uint8_t length_to_read);
//static FILE mystdout = FDEV_SETUP_STREAM(uart_putchar, NULL, _FDEV_SETUP_WRITE);
void delay_ms(uint16_t x);
void delay_us(uint16_t x);
uint16_t ar1000_read(uint8_t address);
void ar1000_write(char reg_address, uint16_t reg_value);
void ar1000_readall(void);
void ar1000_write_array(void);
void ar1000_init(void);
void ar1000_setvolume(uint8_t volume_level);
void ar1000_status(void);
void ar1000_tuneto(uint16_t freq_kHz);
void ar1000_tune_hilo(uint16_t freq_kHz);
void ar1000_seek(void);
uint16_t ar1000_rssi(void);
void print_array(void);
void set_array_value(void);
//RSSI 49-54 is pretty good. 34-41 is complete static
//Register conaining default values for the AR1000, these are the default values from the programming guide.
uint16_t register_values[18] =
{
0xFFFF, //R0
0x5B15, //R1
0xF4B9, //R2 Tune/Channel
0x8012, //R3 seekTHD = 18
0x0400, //R4
0x28AA, //R5
0x4400, //R6
0x1EE7, // R7
0x7141, // R8
0x007D, // R9
0x82C6, // R10 disable wrap
0x4F55, // R11. <--- (disable xo_output)
0x970C, // R12.
0xB845, // R13
0xFC2D, // R14 : Volume control 2
0x8097, // R15
0x04A1, // R16
0xDF6A // R17
//Bad values from the Airoha example code - they don't work for me
/*0xFF7B, // R0 -- the first writable register . (disable xo_en)
0x5B15, // R1
0xD0B9, // R2
0xA010, // R3 seekTHD = 16
0x0780, // R4
0x28AB, // R5
0x6400, // R6
0x1EE7, // R7
0x7141, // R8
0x007D, // R9
0x82C6, // R10 disable wrap
0x4F55, // R11. <--- (disable xo_output)
0x970C, // R12.
0xB845, // R13
0xFC2D, // R14 : Volume control 2
0x8097, // R15
0x04A1, // R16
0xDF6A */ // R17
};
// volume control (increasing)
unsigned char AR1000vol[22] =
{
0x0F, // step 0
0xCF, // 1
0xDF, // 2
0xEF, // 3
0xFF, // 4
0xEE, // 5
0xFE, // 6
0xED, // 7
0xFD, // 8
0xFB, // 9
0xFA, // 10
0xF9, // 11
0xF7, // 12
0xE6, // 13
0xF6, // 14
0xE5, // 15
0xF5, // 16
0xE3, // 17
0xF3, // 18
0xF2, // 19
0xF1, // 20
0xF0 // 21 <------ default setting
};
//======================
// create a FILE structure to reference our UART output function
static FILE uartout = {0} ;
char vol = 15;
char buffer[256] = "initialvalue";
char *pos = buffer;
int station = 879;
void setup(){
// Start the UART
Serial.begin(9600) ;
// fill in the UART file descriptor with pointer to writer.
fdev_setup_stream (&uartout, uart_putchar, NULL, _FDEV_SETUP_WRITE);
ioinit(); //Setup IO pins and defaults
ar1000_tuneto(917);
}
void loop(){
// Load serial data into buffer
if(Serial.available()){
*pos = Serial.read();
if(*pos != '.' && *pos != '#'){
pos++;
}
}
// reset pointer and tune radio
if(*pos == '#'){
*pos = '\0';
pos = buffer;
Serial.print("Tuning: ");
Serial.println(buffer);
station = atoi(buffer);
ar1000_tuneto(station);
}
// next station no wrap, no filter
if(buffer[0] == ']'){
pos = buffer;
*pos = ' ';
Serial.print("Tuning: ");
if(station < MAX_S16)station++;
Serial.println(station, DEC);
ar1000_tuneto(station);
}
// previous station no wrap, no filter
if(buffer[0] == '['){
pos = buffer;
*pos = ' ';
Serial.print("Tuning: ");
if(station > 0) station--;
Serial.println(station, DEC);
ar1000_tuneto(station);
}
// next station incremental, filtered
if(buffer[0] == '='){
pos = buffer;
*pos = ' ';
Serial.print("Tuning: ");
station += 2;
// god filter
while(station == 881 || station == 953 || station == 967 || station == 997 || station == 999 || station == 1003)
station += 2;
if(station > 1079) station = 879;
Serial.println(station, DEC);
ar1000_tuneto(station);
}
// previous station incremental, filtered
if(buffer[0] == '-'){
pos = buffer;
*pos = ' ';
Serial.print("Tuning: ");
station -= 2;
// god filter
while(station == 881 || station == 953 || station == 967 || station == 997 || station == 999 || station == 1003)
station -= 2;
if(station < 879) station = 1079;
Serial.println(station, DEC);
ar1000_tuneto(station);
}
// sudo seek next, filtered
if(buffer[0] == 'n'){
pos = buffer;
*pos = ' ';
Serial.print("Tuning: ");
station += 2;
// sudo seek w/ idiot filter
while(station != 889 && station != 897 && station != 905 && station != 917 && station != 921 && station != 929 && station != 941 && station != 949 && station != 959 && station != 965 && station != 975 && station != 991 && station != 1007 && station != 1013 && station != 1017 && station != 1047 && station != 1061 && station != 1073){
station += 2;
if(station > 1079) station = 879;
delay(100); // for fun
ar1000_tuneto(station); // seems dumb, but large changes cause signal lose for some reason
}
Serial.println(station, DEC);
}
// sudo seek previous, filtered
if(buffer[0] == 'p'){
pos = buffer;
*pos = ' ';
Serial.print("Tuning: ");
station -= 2;
// sudo seek w/ idiot filter
while(station != 889 && station != 897 && station != 905 && station != 917 && station != 921 && station != 929 && station != 941 && station != 949 && station != 959 && station != 965 && station != 975 && station != 991 && station != 1007 && station != 1013 && station != 1017 && station != 1047 && station != 1061 && station != 1073){
station -= 2;
if(station < 879) station = 1079;
delay(100); // for fun
ar1000_tuneto(station); // seems dumb, but large changes cause signal lose for some reason
}
Serial.println(station, DEC);
}
// increase volume 21 MAX
if(buffer[0] == 'u'){
pos = buffer;
*pos = ' ';
if(vol < 21)
vol++;
Serial.print("Volume: ");
Serial.println(vol, DEC);
ar1000_setvolume(vol);
}
// decrease volume 0 MIN
if(buffer[0] == 'd'){
pos = buffer;
*pos = ' ';
if(vol > 0)
vol--;
Serial.print("Volume: ");
Serial.println(vol, DEC);
ar1000_setvolume(vol);
}
}
uint16_t ar1000_rssi(void)
{
#define ADDR_RSSI 0x12
#define MASK_RSSI 0xFE00
#define SHIFT_RSSI 9
uint16_t rssi;
rssi = ar1000_read(ADDR_RSSI);
rssi &= MASK_RSSI;
rssi >>= 9;
return(rssi);
}
// Volume Control
// There are two different fields about volume control in AR1000F
// Volume : D7~D10 in register R3
// Volume2 : D12~D15 in register R14
// 22 combinations of (volume2 + volume) are recommended.
void ar1000_setvolume(uint8_t volume_level)
{
uint16_t reg3, reg14;
reg3 = ar1000_read(3) & 0xF87F; //Zero out bits D7-D10
reg3 |= ( (AR1000vol[volume_level] & 0x0F) << 7); //Mask in D7-D10
reg14 = ar1000_read(14) & 0x0FFF; //Zero out bits D12-D15
reg14 |= ((AR1000vol[volume_level] & 0xF0) << 8); //Mask in D12-D15
ar1000_write(3, reg3);
ar1000_write(14, reg14);
}
//Tunes the AR1000 to a given station.
//Calculate AR1000 CHAN id : Freq (MHz) = 69 + 0.1*CHAN
//Example, sending 973 will tune to 97.3MHz
void ar1000_tuneto(uint16_t freq_kHz)
{
uint16_t channel, temp;
/*
1) Set hmute Bit
2) Clear TUNE Bit
3) Clear SEEK Bit
4) Set BAND/SPACE/CHAN Bits
5) Enable TUNE Bit
6) Wait STC flag (Seek/Tune Comlete, in Status Register
7) Clear hmute Bit
8) Update Functions (optional)
*/
//Clear tune bit
AR1000_TUNE_OFF;
//Set Channel
channel = freq_kHz - 690;
temp = ar1000_read(2); //Read
temp &= 0xFE00; //Mask
temp |= channel;
ar1000_write(2, temp); //Write
//Enable tune bit
AR1000_TUNE_ON;
//Wait for tune to stabilize (STC flag)
temp = 0;
while(temp == 0)
{
temp = ar1000_read(ADDR_STATUS) & MASK_STC;
// printf("!");
}
}
//This is some weird function in AR1000 example code provided by Airoha
//Looks like it takes the RSSI into account and then fine tunes the station
//I can't hear much of a difference, but it looks fancy.
void ar1000_tune_hilo(uint16_t freq_kHz)
{
uint16_t temp;
AR1000_MUTE_ON; //Set mute ON before TUNE
AR1000_SEEK_OFF; //Clear seek
//Read Low-Side LO Injection
//R11 --> clear D15, clear D0/D2, D3 is the same as default
temp = ar1000_read(11) & 0x7FFA;
ar1000_write(11, temp);
//TUNE to FreqKHz with current setting
ar1000_tuneto(freq_kHz); //This function turns on TUNE and waits for STC flag
//Low-side TUNE Ends
printf("\nLow complete");
uint16_t arStatus = ar1000_read(ADDR_RSSI);
uint16_t rssi = (arStatus & MASK_RSSI);
printf("\nRSSI 1 = %d", rssi >> SHIFT_RSSI);
//Read Hi-Side LO Injection
// R11-->set D15, set D0/D2, D3 is the same as default
temp = ar1000_read(11) | 0x8005;
ar1000_write(11, temp);
//TUNE to FreqKHz with current setting
ar1000_tuneto(freq_kHz); //This function turns on TUNE and waits for STC flag
//High-side TUNE Ends
printf("\nHigh complete");
arStatus = ar1000_read(ADDR_RSSI);
printf("\nRSSI 2 = %d", (arStatus & MASK_RSSI) >> SHIFT_RSSI);
rssi = rssi - (arStatus & MASK_RSSI);
if (rssi < 0) //errata in 0.82
{
// LO
// R11--> clear D15, set D0/D2, D3 is the same as default
temp = (ar1000_read(11) & 0x7FFF) | 0x0005;
ar1000_write(11, temp);
}
else
{
//HI
//R11--> set D15, clear D0/D2, D3 is the same as default
temp = (ar1000_read(11) | 0x8000) & 0xFFFA;
ar1000_write(11, temp);
}
//Fine-tune!!
//TUNE to FreqKHz with current setting
ar1000_tune_hilo(freq_kHz); //This function turns on TUNE and waits for STC flag
AR1000_MUTE_OFF;
printf("\nLow/Hi tuning complete");
}
//Starts scanning the stations for a minimum set threshold. I found the bit to enable
//wrapping so the every time the function is called, it searches up, and wrap back to 88MHz
//if it doesn't find a good station.
void ar1000_seek(void)
{
#define ADDR_SEEK_SETTING 0x11
#define SEEK_SETTING 0x2000
#define SEEK_MASK 0xC3FF
#define SEEK_TH_MASK 0xFF80
#define SEEK_TH 5 //A higher threshold causes stronger stations to be found
uint16_t temp;
char space = 1; //0.1MHz scanning
char updown = 1; //Seek up
char band = 0; //US/Europe radio band
AR1000_MUTE_ON;
AR1000_TUNE_OFF;
AR1000_SEEK_OFF;
//Enable wrap during seek - I found bit D3 enables wrap, by trial and error. Seems to work
temp = ar1000_read(10) | (1<<3); //0x82C6 = 1000 0010 1100 0110
ar1000_write(10, temp);
//Setting before seek
temp = (ar1000_read(17) & SEEK_MASK) | SEEK_SETTING;
ar1000_write(17, temp);
printf("\n\nBegin searching:");
AR1000_SEEK_ON;
temp = ar1000_read(3);
if(space == 1) temp |= (1<<13); //Set space
if(updown == 1) temp |= (1<<15); //Set seek up or down
temp = (temp & 0xE7FF) | band; //Set Band
temp &= SEEK_TH_MASK; //Clear out the seek threshold
temp |= SEEK_TH; //Set threshold
ar1000_write(3, temp);
//Wait for tune to stabilize (STC flag)
temp = 0;
while(temp == 0)
{
temp = ar1000_read(ADDR_STATUS) & MASK_STC;
// printf(".");
}
temp = ar1000_read(ADDR_STATUS) & MASK_SF;
if(temp != 0)
{
printf("\nSeek failed!");
return;
}
printf("\nSeek success!");
temp = ar1000_read(ADDR_STATUS) & MASK_READCHAN;
uint16_t freq_kHz = 690 + (temp >> SHIFT_READCHAN); //Determine what channel we found
printf("\nNow on channel %d.%dMHz", freq_kHz / 10, freq_kHz % 10);
//Restore setting after seek
ar1000_write(17, register_values[17]);
//Fine-tune with auto hilo rejection
ar1000_tuneto(freq_kHz);
AR1000_MUTE_OFF;
}
//This function reads in an address and array value, and stores the value into the array address
//it does not change the values in the ar1000, you will need to use the "send array valus"
//function in order to send the new values to the ar1000
void set_array_value(void)
{
uint8_t array_address;
uint16_t array_value;
printf("\n\nArray Address (2 digit hex value): ");
array_address = uart_gethex(2);
printf("\nArray Address is: %x", array_address);
printf("\n\nArray value (4 digit hex value): ");
array_value = uart_gethex(4);
printf("\nArray value is: %x", array_value);
register_values[array_address] = array_value;
}
void print_array(void)
{
//prints the values of the array that is used to control the radio
printf("\n\nArray position: value\n");
for(int i = 0 ; i < 18 ; i++)
printf("0x%.2X: 0x%.4X\n", i, register_values[i]);
}
//Reads a memory register from the AR1000
uint16_t ar1000_read(uint8_t address_to_read)
{
char byte1 = 0, byte2 = 0;
char ack;
AGAIN:
i2c_SendStart(); //Send start condition
ack = i2c_SendByte(AR1000_W); //Send slave device address with write
ack &= i2c_SendByte(address_to_read); //Send address to read
if(ack == 0)
{
#ifdef I2CDEBUG
printf("!"); //No ACK!
#endif
goto AGAIN;
}
i2c_SendStart(); //Send start condition
i2c_SendByte(AR1000_R); //Ask device to read the value at the requested address
if(inb(TWSR) == TW_MR_SLA_ACK)
{
byte1 = i2c_ReceiveByte(TRUE);
byte2 = i2c_ReceiveByte(TRUE);
}
else
{
// device did not ACK it's address,
// data will not be transferred
// return error
//retval = I2C_ERROR_NODEV;
printf("\n\tAck failed!");
}
i2c_SendStop();
//Combine two bytes into one 16-bit word
int16_t temp = byte1 << 8;
temp |= byte2;
return(temp);
}
void ar1000_write(char reg_address, uint16_t reg_value)
{
char ack;
uint8_t value1 = (reg_value & 0xFF00) >> 8;
uint8_t value2 = (reg_value & 0x00FF);
AGAIN:
i2c_SendStart(); //Send start condition
ack = i2c_SendByte(AR1000_W);
ack &= i2c_SendByte(reg_address); //Send address to write to
ack &= i2c_SendByte(value1); //Send the two data bytes to be stored
ack &= i2c_SendByte(value2);
i2c_SendStop();
if(ack == 0)
{
#ifdef I2CDEBUG
printf("!"); //No ACK!
#endif
goto AGAIN;
}
}
void ar1000_write_array(void)
{
// This code writes the array values to the ar1000, it is used to calibrate the ar1000
// on power up and it can send the modified array values needed for the seeking tuning etc
//The example AR1000 code disables the analog and digital blocks
// then write to the 0x01 to 0x11 registers
// then enables the analog and digital blocks - so that's what we will do as well
//Write the first register
ar1000_write(0, register_values[0] & 0xFFFE); //<--- Notice we force the enable bit to zero
for(int i = 1 ; i < 18 ; i++)
ar1000_write(i, register_values[i]); //Write registers 1 to 17 to AR1000
ar1000_write(0, register_values[0]); //Re-write the first register, this will set the enable bit
}
//Reads and prints all 16 registers (16-bits wide) of the AR1000
void ar1000_readall(void)
{
uint16_t x, register_value;
for(x = 0 ; x < 0x1D ; x++)
{
register_value = ar1000_read(x);
printf("0x%.2X: 0x%.4X\n", x, register_value);
}
}
void ar1000_init(void)
{
delay_ms(100); //Wait for power to stabilize
ar1000_write_array(); //Init the AR1000 by writing the initial recommended values
uint16_t arStatus = 0;
while(arStatus == 0)
{
arStatus = ar1000_read(ADDR_STATUS);
printf("\nAR1000 arStatus : 0x%04X", arStatus);
arStatus = arStatus & MASK_STC;
delay_ms(10);
}
}
//Read the arStatus register (0x13) of the AR1000
void ar1000_status(void)
{
uint16_t arStatus;
arStatus = ar1000_read(ADDR_STATUS);
printf("\n\nAR1000 arStatus : 0x%04X", arStatus);
uint16_t channel = arStatus & MASK_READCHAN;
channel >>= SHIFT_READCHAN;
channel += 690;
printf("\nChannel : %02d.%01dMHz", channel / 10, channel % 10);
if(arStatus & MASK_STC)
printf(" (Seek/Tune Complete)");
else
printf(" (Seek/Tune Incomplete)");
if(arStatus & MASK_SF)
printf(" (Seek Fail)");
else
printf(" (Seek Successful)");
if(arStatus & MASK_ST)
printf(" (Stereo)");
else
printf(" (Mono)");
}
//Setup for UART and IO pins
void ioinit (void)
{
//1 = output, 0 = input
DDRB = 0b11111111; //All outputs
DDRC = 0b11111111; //All outputs
//DDRD = 0b11111110; //PORTD (RX on PD0)
// stdout = &mystdout; //Required for printf init
// The uart is the standard output device STDOUT.
stdout = &uartout ;
/*
UBRR0H = (MYUBRR) >> 8;
UBRR0L = MYUBRR;
UCSR0B = (1<<RXEN0)|(1<<TXEN0);
UCSR0C = (3<<UCSZ00);
UCSR0A = (1<<U2X0);
*/
//Init timer 0 for delay_us timing
//8,000,000 / 8 = 1,000,000
TCCR0B = (1<<CS01); //Set Prescaler to 8. CS01=1
//initialize I2C hardware
TWCR = 0x00;
TWBR = 64;
//TWSR = (1 << TWPS1);
cbi(TWCR, TWEA);
sbi(TWCR, TWEN);
ar1000_init(); //Initialize AR1000
}
/*
static int uart_putchar(char c, FILE *stream)
{
if (c == '\n') uart_putchar('\r', stream);
loop_until_bit_is_set(UCSR0A, UDRE0);
UDR0 = c;
return 0;
}
*/
// create a output function
// This works because Serial.write, although of
// type virtual, already exists.
static int uart_putchar (char c, FILE *stream)
{
Serial.write(c) ;
return 0 ;
}
/*
uint8_t uart_getchar(void)
{
while( !(UCSR0A & (1<<RXC0)) );
return(UDR0);
}
*/
uint8_t uart_getchar(void){
UDR0 = Serial.read();
return(UDR0);
}
//Reads in ASCII characters, converts to decimal and returns decimal variable
//length_to_read is how many characters we want to read, "A33C" would be four characters long
int uart_gethex(uint8_t length_to_read)
{
int decimal_value = 0;
unsigned char input_character;
for(uint8_t x = 0 ; x < length_to_read ; x++)
{
decimal_value <<= 4; //Every time we loop, make room for another 4-bit hex value to be masked into decimal_value
input_character = uart_getchar();
printf("%c", input_character);
//Check the character for validity
if( (input_character >= '0') && (input_character <= '9') )
decimal_value |= (input_character - '0');
else if( (input_character >= 'a') && (input_character <= 'f') )
decimal_value |= (input_character - 'a');
else
{
//We have a non-legal character. Handle the exception however you want
return(0);
}
}
return(decimal_value);
}
//General short delays
//general short delays
//Uses internal timer do a fairly accurate 1us
//Because we are using 16MHz and a prescalar of 8 on Timer0, we have to double x
void delay_us(uint16_t x)
{
while(x > 256)
{
TIFR0 = (1<<TOV0); //Clear any interrupt flags on Timer0
TCNT0 = 0; //Preload Timer0 for 256 clicks. Should be 1us per click
while( (TIFR0 & (1<<TOV0)) == 0);
x -= 256;
}
TIFR0 = (1<<TOV0); //Clear any interrupt flags on Timer0
TCNT0 = 256 - x; //256 - 125 = 131 : Preload Timer0 for x clicks. Should be 1us per click
while( (TIFR0 & (1<<TOV0)) == 0);
}
//General short delays
void delay_ms(uint16_t x)
{
for ( ; x > 0 ; x--)
delay_us(1000);
}
//==========================
//
//I2C functions
//
//==========================
void i2c_SendStart(void)
{
// send start condition
TWCR = (1<<TWINT)|(1<<TWSTA)|(1<<TWEN);
i2c_WaitForComplete();
}
void i2c_SendStop(void)
{
// transmit stop condition
TWCR = (1<<TWSTO);
}
void i2c_WaitForComplete(void)
{
// wait for any previous i2c stuff to complete before sending new data
while (!(TWCR & (1<<TWINT)));
}
unsigned char i2c_SendByte(unsigned char data)
{
// save data to the TWDR
TWDR = data;
// begin send
TWCR = (1<<TWINT)|(1<<TWEN);
// wait until transmission completed
while(!(TWCR & (1<<TWINT)));
// check value of TWI Status Register. Mask prescaler bits
uint8_t twst = TWSR & 0xF8;
#ifdef I2CDEBUG
printf("twst: 0x%02X\n\n", twst);
#endif
if( twst == 0x18) return 1; //SKA+W was tranmitted, ACK received
if( twst == 0x28) return 1; //Data was tranmitted, ACK received
return 0;
}
unsigned char i2c_ReceiveByte(unsigned char ackFlag)
{
// begin receive over i2c
if( ackFlag )
{
// ackFlag = TRUE: ACK the recevied data
outb(TWCR, (inb(TWCR)&TWCR_CMD_MASK)|BV(TWINT)|BV(TWEA));
}
else
{
// ackFlag = FALSE: NACK the recevied data
outb(TWCR, (inb(TWCR)&TWCR_CMD_MASK)|BV(TWINT));
}
i2c_WaitForComplete();
// retieve received data byte from i2c TWDR
return( inb(TWDR) );
}