- Mon Nov 30, 2009 6:54 am
#86191
waltr wrote:I get the "unable to communicate with modem" message when the baud rate is wrong or the #bits is wrong and the module is in AT command mode.Thanks for the suggestion. I've gone through all the baud rate options (in the drop down) without any success. I am inclined to think that it is not a baud rate issue, because when set to 9600 I can get an "OK" response ocassionally in the terminal tab. It always happens after resetting the module (shorting the RST to GND) and doesn't happen consistently.
I get "name unknown (ID=42949672481228316)" if the module is in AT mode and the API box is checked. I also get this message with a module in API mode and the baud rate is wrong.
Keep trying different baud rates with and without the API box checked.